<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Question on TJA1043 in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Question-on-TJA1043/m-p/1153633#M17438</link>
    <description>&lt;P&gt;Can you please explain a little bit more detail about why the device pulls INH pin up to VBAT when the VBAT is applied ?&lt;/P&gt;&lt;P&gt;Is this because the pins VBatt &amp;amp; Wake are tied together ? Is the device considering this as a local wake-up event ?&lt;/P&gt;</description>
    <pubDate>Tue, 15 Sep 2020 18:29:50 GMT</pubDate>
    <dc:creator>nadeem_syed</dc:creator>
    <dc:date>2020-09-15T18:29:50Z</dc:date>
    <item>
      <title>Question on TJA1043</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Question-on-TJA1043/m-p/1153094#M17435</link>
      <description>&lt;P&gt;In our application, pins VBAT (pin 10) and WAKE (pin 9) are tied together. Our application matches with the information shown in Section.12 Example Application diagram of datasheet.&lt;/P&gt;&lt;P&gt;I have following question&lt;/P&gt;&lt;P&gt;1. When we provide VBATT (12V) to our application we are observing "INH" signal turns on.&lt;BR /&gt;I believe TJA1043 device considers this as a local wake-up event and turns on "INH" signal. Is my understanding correct ?&lt;BR /&gt;&lt;BR /&gt;2. What will be the operating mode of TJA1043 device when VBATT is turned off ?&lt;/P&gt;</description>
      <pubDate>Tue, 15 Sep 2020 01:01:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Question-on-TJA1043/m-p/1153094#M17435</guid>
      <dc:creator>nadeem_syed</dc:creator>
      <dc:date>2020-09-15T01:01:10Z</dc:date>
    </item>
    <item>
      <title>Re: Question on TJA1043</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Question-on-TJA1043/m-p/1153456#M17437</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1) when Vbat is applied, transceiver goes to Standby mode, INH pin is pulled up to Vbat. Once EN and STBN pins becomes driven by the MCU, a mode is determined by their level, for example if driven high transceiver enters Normal mode.&lt;/P&gt;
&lt;P&gt;2) if there is undervoltage only on Vbat then device is in Standby mode. If there is undervoltage on Vio or Vcc then device go to Sleep mode.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;See more in AH1014;&amp;nbsp;&lt;A href="https://www.nxp.com/documents/report/AH1014_v1_4_Application_Hints_TJA1042_43_48_51.pdf" target="_blank"&gt;https://www.nxp.com/documents/report/AH1014_v1_4_Application_Hints_TJA1042_43_48_51.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Sep 2020 11:08:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Question-on-TJA1043/m-p/1153456#M17437</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2020-09-15T11:08:05Z</dc:date>
    </item>
    <item>
      <title>Re: Question on TJA1043</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Question-on-TJA1043/m-p/1153633#M17438</link>
      <description>&lt;P&gt;Can you please explain a little bit more detail about why the device pulls INH pin up to VBAT when the VBAT is applied ?&lt;/P&gt;&lt;P&gt;Is this because the pins VBatt &amp;amp; Wake are tied together ? Is the device considering this as a local wake-up event ?&lt;/P&gt;</description>
      <pubDate>Tue, 15 Sep 2020 18:29:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Question-on-TJA1043/m-p/1153633#M17438</guid>
      <dc:creator>nadeem_syed</dc:creator>
      <dc:date>2020-09-15T18:29:50Z</dc:date>
    </item>
    <item>
      <title>Re: Question on TJA1043</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Question-on-TJA1043/m-p/1155314#M17441</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;transceiver's behavior after Vbat connection is described in chapter "Software flow for an ECU cold start" of AH1014 (page 67).&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Petr&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 18 Sep 2020 06:45:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Question-on-TJA1043/m-p/1155314#M17441</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2020-09-18T06:45:07Z</dc:date>
    </item>
  </channel>
</rss>