<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Re: GDU VLS threshold</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/GDU-VLS-threshold/m-p/1094520#M17406</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/pratibhasurabhi"&gt;pratibhasurabhi&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&lt;BR /&gt;Yes, there should be: &lt;BR /&gt;0 = VLS_OUT pin voltage is above VLVLSHD or VLVLSLD&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.&lt;BR /&gt;There is a hysteresis although it is not specified.&lt;BR /&gt;You can see that the typical deassert level is a bit higher than the assert level.&lt;BR /&gt;So, it should not flag the error immediately, the VLS_OUT voltage would need to drop.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Jul 2020 09:27:50 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2020-07-28T09:27:50Z</dc:date>
    <item>
      <title>GDU VLS threshold</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/GDU-VLS-threshold/m-p/1094519#M17405</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using ZVML64 with GDUV4. From the RM v2.13, the voltage thresholds for undervoltage on VLS for GDU V4 are VLVLSHA and VLVLSHD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Under the GDUF register description , for GLVLSF bit , for bit value 0 -&amp;gt;VLS_OUT pin voltage is above VLVLSD&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question 1) My understanding is that VLVLSD is nothing but VLVLSHD. It is an prinitng error. Can anyone please confirm the same.?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question 2) After having a quick look at the GDU electrical characteristics table for V4 for&amp;nbsp;VLVLSHA and&amp;nbsp;VLVLSHD [10a and 10b respectively], I can see that the min,typ and max voltage levels are almost overlapping if not equal.&lt;/P&gt;&lt;P&gt;My thinking is that; due to these overlapping thresholds, the GLVLSF bit will set immediately once it is cleared or viceversa [if the voltages are at that detection level]&lt;/P&gt;&lt;P&gt;Can someone please explain if these overlapping levels are ok and reason for the overlapping voltage levels.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jul 2020 06:25:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/GDU-VLS-threshold/m-p/1094519#M17405</guid>
      <dc:creator>pratibhasurabhi</dc:creator>
      <dc:date>2020-07-28T06:25:19Z</dc:date>
    </item>
    <item>
      <title>Re: GDU VLS threshold</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/GDU-VLS-threshold/m-p/1094520#M17406</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/pratibhasurabhi"&gt;pratibhasurabhi&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&lt;BR /&gt;Yes, there should be: &lt;BR /&gt;0 = VLS_OUT pin voltage is above VLVLSHD or VLVLSLD&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.&lt;BR /&gt;There is a hysteresis although it is not specified.&lt;BR /&gt;You can see that the typical deassert level is a bit higher than the assert level.&lt;BR /&gt;So, it should not flag the error immediately, the VLS_OUT voltage would need to drop.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jul 2020 09:27:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/GDU-VLS-threshold/m-p/1094520#M17406</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-07-28T09:27:50Z</dc:date>
    </item>
  </channel>
</rss>