<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S12ZVL Port AD interrupt in Stop Mode in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL-Port-AD-interrupt-in-Stop-Mode/m-p/1020535#M17035</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/RadekS"&gt;RadekS&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your suggestions. I will modify the code as per your suggestions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to use analog pin only.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this scenario can I use Autonomous Periodical Interrupt method?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Feb 2020 14:56:46 GMT</pubDate>
    <dc:creator>chaitanya_kalyani</dc:creator>
    <dc:date>2020-02-17T14:56:46Z</dc:date>
    <item>
      <title>S12ZVL Port AD interrupt in Stop Mode</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL-Port-AD-interrupt-in-Stop-Mode/m-p/1020531#M17031</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In our project, we are reading switches using analog(Port AD)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My requirement is to wake up MCU from stop mode when the switch is pressed longer than 20ms.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I implement this?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you provide me some example to wake up MCU from stop mode when the switch is pressed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Feb 2020 06:42:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL-Port-AD-interrupt-in-Stop-Mode/m-p/1020531#M17031</guid>
      <dc:creator>chaitanya_kalyani</dc:creator>
      <dc:date>2020-02-13T06:42:20Z</dc:date>
    </item>
    <item>
      <title>Re: S12ZVL Port AD interrupt in Stop Mode</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL-Port-AD-interrupt-in-Stop-Mode/m-p/1020532#M17032</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN style="font-size: 9.0pt; color: #646464; background: white;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="351656" data-username="chaitanya.kalyani@seoyonelec-rnd.in" href="https://community.nxp.com/people/chaitanya.kalyani@seoyonelec-rnd.in"&gt;&lt;SPAN style="border: none windowtext 1.0pt; padding: 0in; color: #3d9ce7; background: white; text-decoration: none; font-size: 9.0pt;"&gt;&lt;STRONG&gt;Chaitanya&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;There are more options for how to solve it.&lt;/P&gt;&lt;P&gt;The first option is using port interrupt with wake-up capability. Unfortunately, this interrupt may detect only a single edge type in the time (falling or rising). The edge type may be changed runtime, however, it is not an atomic operation and it might fail due to glitches at such asynchronous source like a push-button (we may simply miss next edge).&lt;/P&gt;&lt;P&gt;A partial workaround is detection just first edge (e.g. falling edge) and waits 20ms before a simple test of pin logic value. For these 20ms we may use any already initialized periodic interrupt or use one output compare timer channel.&lt;/P&gt;&lt;P&gt;The pins with interrupt and key-wakeup capability (Ports AD, S, P and L at S12ZVL) already contain a digital filter on each pin that prevents short pulses from generating an interrupt. A valid edge on an input is detected if 4 consecutive samples of a passive level are followed by 4 consecutive samples of an active level. Else the sampling logic is restarted. However, this does not fit with the requested 20ms interval (it is just at least 10us for MCU in stop mode).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The more robust solution is using any pin routed to the timer (port T, optionally rerouted to the port P or S). The timer may detect both edges and the time between them may by measured preciously. This allows also do an action only when push button is really released. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I attached simple example codes for the timer – generating intervals via output compare and time measurement via input capture.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Of course, there may be more ways how to do it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Radek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Feb 2020 14:39:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL-Port-AD-interrupt-in-Stop-Mode/m-p/1020532#M17032</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2020-02-13T14:39:10Z</dc:date>
    </item>
    <item>
      <title>Re: S12ZVL Port AD interrupt in Stop Mode</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL-Port-AD-interrupt-in-Stop-Mode/m-p/1020533#M17033</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/RadekS"&gt;RadekS&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I implemented using&amp;nbsp;Pin interrupts and Key-Wakeup (KWU). It is working fine for SW8 but it is not working for SW9.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My primary assumption is when we press a switch that time not getting the required voltage level.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I implemented it as follows.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void GoToSleep(void)&lt;BR /&gt;{&lt;BR /&gt; DisableInterrupts;&lt;BR /&gt; //Digital Input Function Enable --[1] digital in [0] analog in&lt;BR /&gt; DIENADL_DIENADL0 = 1;&lt;BR /&gt; __asm(CLI);&lt;BR /&gt; __asm(ANDCC #0x7F); // CCW settings: S = 0, I = 0 &lt;BR /&gt; SCI0ASR1_RXEDGIF = 1; // clear flag&lt;BR /&gt; SCI0ACR1_RXEDGIE = 1; // edge interrupt enabled for wake up&lt;BR /&gt; //Interrupt enable register - [1] Enable [0] Disable&lt;BR /&gt; PIEAD_PIEADL0 = 1;&lt;BR /&gt; //Select Polarity&lt;BR /&gt; //1 - Pull-down device selected; rising edge selected&lt;BR /&gt; //0 - 0 Pull-up device selected; falling edge selected&lt;BR /&gt; PPSAD_PPSADL0 = 0;&lt;BR /&gt; EnableInterrupts;&lt;BR /&gt; __asm(STOP);&lt;BR /&gt; //After come out of stop mode disable interrupts&lt;BR /&gt; SCI0ACR1_RXEDGIE = 0;&lt;BR /&gt; SCI0ACR1_RXEDGIE = 0;&lt;BR /&gt; //Analog In&lt;BR /&gt; DIENADL_DIENADL0 = 0;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#pragma CODE_SEG __NEAR_SEG NON_BANKED&lt;BR /&gt;ISR(IntPortAD)&lt;BR /&gt;{&lt;BR /&gt; if (PIFADL_PIFADL1 == 1&lt;BR /&gt; {&lt;BR /&gt; PIFADL_PIFADL0 = 1;&lt;BR /&gt; l_ifc_wake_up(LI0);&lt;BR /&gt;State = Operating;&lt;BR /&gt; }&lt;BR /&gt;}&lt;BR /&gt;#pragma CODE_SEG DEFAULT&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please suggest to me if you have any alternate solution or need some modification from the SW/HW side.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Feb 2020 10:39:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL-Port-AD-interrupt-in-Stop-Mode/m-p/1020533#M17033</guid>
      <dc:creator>chaitanya_kalyani</dc:creator>
      <dc:date>2020-02-15T10:39:32Z</dc:date>
    </item>
    <item>
      <title>Re: S12ZVL Port AD interrupt in Stop Mode</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL-Port-AD-interrupt-in-Stop-Mode/m-p/1020534#M17034</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="351656" data-username="chaitanya.kalyani@seoyonelec-rnd.in" href="https://community.nxp.com/people/chaitanya.kalyani@seoyonelec-rnd.in" style="color: #3d9ce7; background-color: #ffffff; border: 0px; font-weight: 200; text-decoration: underline; font-size: 1.286rem;"&gt;Chaitanya&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Yes, the problem with the voltage level make sense.&lt;/P&gt;&lt;P&gt;If we assume resistor values according to the scheme in this thread, then:&lt;/P&gt;&lt;P&gt;SW8=OFF, SW9=OFF&amp;nbsp; &amp;nbsp;Vad0=VDDX&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;SW8=OFF, SW9=ON&amp;nbsp; &amp;nbsp; &amp;nbsp;Vad0=VDDX*(820+1500)/(820+1500+3000)=0.44*VDDX&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;SW8=ON, SW9=OFF&amp;nbsp; &amp;nbsp; &amp;nbsp;Vad0=VDDX*(820)/(820+3000)=0.21VDDX&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The influence of the MCU internal impedance will be rather negligible in this case.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;According to the reference manual, the maximum low voltage is 0.35*VDDX for 5V VDDX voltage or 0.3*VDDX for 3.3V VDDX voltage&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Just a few notes regarding your code:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1. the &lt;SPAN&gt;EnableInterrupts;&lt;/SPAN&gt;&amp;nbsp;macro is the same as&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;__asm(CLI);&lt;/SPAN&gt;&lt;BR style="color: #51626f; background-color: #ffffff;" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;So, we may remove the&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;__asm(CLI);&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN&gt;line.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I would like to recommend enable interrupts just prior STOP instruction for avoiding interrupt triggers before STOP mode initialization. Lines&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;EnableInterrupts; directly followed by&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;__asm(STOP);&lt;/SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;are correct.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2. You don't need to clear S-bit in every STOP mode entry. It may be part of MCU's initialization (just once after MCU reset).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;3. If you use this AD pin just for wake-up (no analog), you may set up a digital buffer once during&amp;nbsp;initialization.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;4. I would like to recommend strictly not use commands like&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;PIFADL_PIFADL0 = 1;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN&gt;for flag clearing (for registers with two or more flags). This command will clear all pending flags in PIFADL register (it is read/modify/write command). Please use for example commands like PIFADL=0x01; or&amp;nbsp;PIFADL =&amp;nbsp;PIFADL_PIFADL0_MASK for clearing single flag. For more details please check &lt;A href="https://www.nxp.com/docs/en/application-note/AN2554.pdf"&gt;AN2554 Clearing and Disabling Interrupt Flags&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I hope it helps you.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Radek&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Feb 2020 14:28:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL-Port-AD-interrupt-in-Stop-Mode/m-p/1020534#M17034</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2020-02-17T14:28:11Z</dc:date>
    </item>
    <item>
      <title>Re: S12ZVL Port AD interrupt in Stop Mode</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL-Port-AD-interrupt-in-Stop-Mode/m-p/1020535#M17035</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/RadekS"&gt;RadekS&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your suggestions. I will modify the code as per your suggestions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to use analog pin only.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this scenario can I use Autonomous Periodical Interrupt method?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Feb 2020 14:56:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL-Port-AD-interrupt-in-Stop-Mode/m-p/1020535#M17035</guid>
      <dc:creator>chaitanya_kalyani</dc:creator>
      <dc:date>2020-02-17T14:56:46Z</dc:date>
    </item>
  </channel>
</rss>