<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Re: maximum ratings for LIN</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/maximum-ratings-for-LIN/m-p/1011767#M16999</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jakob,&lt;/P&gt;&lt;P&gt;It should not damage the MCU, because the LIN standard specifies such a condition as loss of supply.&lt;BR /&gt;Under this condition, the input injection (or leakage) current in the recessive state needs to be very limited by the LIN PHY in order to not disturb the&amp;nbsp;LIN communication for other modules on the bus.&lt;BR /&gt;Please see Table D-1, S12ZVM RM rev.2.13&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/100746i594F20CC37A8AFA1/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;However, there can be some issues.&lt;BR /&gt;Depending on the total resistive load on the bus, the MCU can detect overcurrent in the dominant state.&lt;/P&gt;&lt;P&gt;Also, the LIN PHY slew rate is a function of the supply voltage, e.g. the higher the supply, the faster the rate is in order to have a fixed timing for the slopes.&lt;BR /&gt;Although the bus voltage is higher, the LIN PHY operates&amp;nbsp;at VLINSUP voltage and might not use so appropriate timing, the transmitter may reserve too much time for the slopes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Feb 2020 12:27:19 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2020-02-17T12:27:19Z</dc:date>
    <item>
      <title>maximum ratings for LIN</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/maximum-ratings-for-LIN/m-p/1011766#M16998</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we are using S912ZVML31F1WKF in a 80W BLDC application with LIN communication and I have a question about the LIN Interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What would happen if the Signal Level is higher than the supply voltage? We have an universal test equipment which provides the test&amp;nbsp;LIN interface but this device is driven with 24V&amp;nbsp;and our DUT is only powered with 8 to 16V (Voltage range for 12V car battery) Could this constellation lead into bus failure or even device damage?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your help,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jakob Kleinen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Feb 2020 09:34:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/maximum-ratings-for-LIN/m-p/1011766#M16998</guid>
      <dc:creator>j_kleinen</dc:creator>
      <dc:date>2020-02-12T09:34:38Z</dc:date>
    </item>
    <item>
      <title>Re: maximum ratings for LIN</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/maximum-ratings-for-LIN/m-p/1011767#M16999</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jakob,&lt;/P&gt;&lt;P&gt;It should not damage the MCU, because the LIN standard specifies such a condition as loss of supply.&lt;BR /&gt;Under this condition, the input injection (or leakage) current in the recessive state needs to be very limited by the LIN PHY in order to not disturb the&amp;nbsp;LIN communication for other modules on the bus.&lt;BR /&gt;Please see Table D-1, S12ZVM RM rev.2.13&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/100746i594F20CC37A8AFA1/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;However, there can be some issues.&lt;BR /&gt;Depending on the total resistive load on the bus, the MCU can detect overcurrent in the dominant state.&lt;/P&gt;&lt;P&gt;Also, the LIN PHY slew rate is a function of the supply voltage, e.g. the higher the supply, the faster the rate is in order to have a fixed timing for the slopes.&lt;BR /&gt;Although the bus voltage is higher, the LIN PHY operates&amp;nbsp;at VLINSUP voltage and might not use so appropriate timing, the transmitter may reserve too much time for the slopes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Feb 2020 12:27:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/maximum-ratings-for-LIN/m-p/1011767#M16999</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-02-17T12:27:19Z</dc:date>
    </item>
    <item>
      <title>Re: maximum ratings for LIN</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/maximum-ratings-for-LIN/m-p/1011768#M17000</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for your help. So far we didn't experience any timing problems but we will change our equipment to prevent problems in the future.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jakob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Feb 2020 12:58:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/maximum-ratings-for-LIN/m-p/1011768#M17000</guid>
      <dc:creator>j_kleinen</dc:creator>
      <dc:date>2020-02-17T12:58:56Z</dc:date>
    </item>
  </channel>
</rss>