<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックS12ZVML128 Sensorless stall error issue</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVML128-Sensorless-stall-error-issue/m-p/986383#M16892</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear&amp;nbsp;friends：&lt;/P&gt;&lt;P&gt;I&amp;nbsp;use&amp;nbsp;the s12zvml128 mcu to drive oil pump BLDC motor.I reference the demo&amp;nbsp;MC9S12ZVML128_BLDC_Sensorless code.&lt;/P&gt;&lt;P&gt;I have an issue about the demo. when I drive the motor, if the load exceed about 0.3N. The controller will trigger the stall&lt;/P&gt;&lt;P&gt;error protection. and the state machine will back to the init. the motor speed will back to the init speed. if I cancel the stall error protection the motor speed will out of control. which make me confused is it happens after speed is stabilized. rather than in start or during loading. ( I am sure the motor is not stalled )&lt;/P&gt;&lt;P&gt;Besides, if the load is light. the controller will not easy trigger this protect. could you tell me why?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Nov 2019 01:16:19 GMT</pubDate>
    <dc:creator>dmeng1</dc:creator>
    <dc:date>2019-11-14T01:16:19Z</dc:date>
    <item>
      <title>S12ZVML128 Sensorless stall error issue</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVML128-Sensorless-stall-error-issue/m-p/986383#M16892</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear&amp;nbsp;friends：&lt;/P&gt;&lt;P&gt;I&amp;nbsp;use&amp;nbsp;the s12zvml128 mcu to drive oil pump BLDC motor.I reference the demo&amp;nbsp;MC9S12ZVML128_BLDC_Sensorless code.&lt;/P&gt;&lt;P&gt;I have an issue about the demo. when I drive the motor, if the load exceed about 0.3N. The controller will trigger the stall&lt;/P&gt;&lt;P&gt;error protection. and the state machine will back to the init. the motor speed will back to the init speed. if I cancel the stall error protection the motor speed will out of control. which make me confused is it happens after speed is stabilized. rather than in start or during loading. ( I am sure the motor is not stalled )&lt;/P&gt;&lt;P&gt;Besides, if the load is light. the controller will not easy trigger this protect. could you tell me why?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Nov 2019 01:16:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVML128-Sensorless-stall-error-issue/m-p/986383#M16892</guid>
      <dc:creator>dmeng1</dc:creator>
      <dc:date>2019-11-14T01:16:19Z</dc:date>
    </item>
  </channel>
</rss>