<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Accessing Global Address in S12G128 in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Accessing-Global-Address-in-S12G128/m-p/970636#M16821</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;S12G128 uses global addresses only in the case of flash Erase or write. For reading you have to use PPAGE_OFFSET addressing mode. Please look into attached example which writes and reads the FLASH at G240.&lt;/P&gt;&lt;P&gt;Using global addresses for Flash E/W are described in the Flash module chapters.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Data sheet:&lt;/P&gt;&lt;P&gt;Expansion of the CPU Local Address Map&lt;BR /&gt;The program page index register in S12GMMC allows accessing up to 256KB of address space in the&lt;BR /&gt;global memory map by using the four index bits (PPAGE[3:0]) to page 16x16 KB blocks into the program&lt;BR /&gt;page window located from address 0x8000 to address 0xBFFF in the local CPU memory map.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know it is "a little bit" hidden.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please look into SW example I attached. You will see the difference between writing and reading the FLASH.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ladislav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Sep 2019 12:45:39 GMT</pubDate>
    <dc:creator>lama</dc:creator>
    <dc:date>2019-09-10T12:45:39Z</dc:date>
    <item>
      <title>Accessing Global Address in S12G128</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Accessing-Global-Address-in-S12G128/m-p/970635#M16820</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;In S12G128, &lt;STRONG&gt;Global addresses&lt;/STRONG&gt; are &lt;STRONG style="text-decoration: underline; "&gt;not accessed&lt;/STRONG&gt; while &lt;STRONG&gt;reading PFLASH&lt;/STRONG&gt;. Why?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Where it is mentioned in the datasheet of S12G128 microcontroller?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kindly answer my question.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Arthi Venkatasubramanian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Sep 2019 09:10:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Accessing-Global-Address-in-S12G128/m-p/970635#M16820</guid>
      <dc:creator>arthivenkatasub</dc:creator>
      <dc:date>2019-09-10T09:10:51Z</dc:date>
    </item>
    <item>
      <title>Re: Accessing Global Address in S12G128</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Accessing-Global-Address-in-S12G128/m-p/970636#M16821</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;S12G128 uses global addresses only in the case of flash Erase or write. For reading you have to use PPAGE_OFFSET addressing mode. Please look into attached example which writes and reads the FLASH at G240.&lt;/P&gt;&lt;P&gt;Using global addresses for Flash E/W are described in the Flash module chapters.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Data sheet:&lt;/P&gt;&lt;P&gt;Expansion of the CPU Local Address Map&lt;BR /&gt;The program page index register in S12GMMC allows accessing up to 256KB of address space in the&lt;BR /&gt;global memory map by using the four index bits (PPAGE[3:0]) to page 16x16 KB blocks into the program&lt;BR /&gt;page window located from address 0x8000 to address 0xBFFF in the local CPU memory map.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know it is "a little bit" hidden.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please look into SW example I attached. You will see the difference between writing and reading the FLASH.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ladislav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Sep 2019 12:45:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Accessing-Global-Address-in-S12G128/m-p/970636#M16821</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2019-09-10T12:45:39Z</dc:date>
    </item>
  </channel>
</rss>