<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: MC9S12ZVL ADC external trigger</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12ZVL-ADC-external-trigger/m-p/967138#M16813</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Edward,&amp;nbsp;&lt;/P&gt;&lt;P&gt;You were right. PE didn't generate the code for pin setting. But in my code there is next issue apart from of this. After set the input pin, there is needed to set the RSTA bit in the ADCFLWCTL register, and in case when restart mode is used (as in my example)&amp;nbsp; when the end of list is reached, the RSTA bit has to be re-set.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 Jul 2019 12:45:00 GMT</pubDate>
    <dc:creator>lukasz_bittner</dc:creator>
    <dc:date>2019-07-26T12:45:00Z</dc:date>
    <item>
      <title>MC9S12ZVL ADC external trigger</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12ZVL-ADC-external-trigger/m-p/967136#M16811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm playing with the DEVKIT-S12ZVL board. What I'm trying to do it's an used an external trigger for ADC. I have created a project in the CW 11.1 with Processor Expert. As a trigger pin I'm using PAD5. To this pin I have connected logic analyzer as well. I have checked that the pin is pulled up.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/83060i2E2DB4ACAE33C987/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But the measuring is not starting. Could someone tell me what I'm doing wrong that I',m not able to start the measure?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jul 2019 14:16:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12ZVL-ADC-external-trigger/m-p/967136#M16811</guid>
      <dc:creator>lukasz_bittner</dc:creator>
      <dc:date>2019-07-25T14:16:49Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S12ZVL ADC external trigger</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12ZVL-ADC-external-trigger/m-p/967137#M16812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't know, should&amp;nbsp;digital input enable (DIENADL) be set for PAD5 when uses as an&amp;nbsp;ETRIG? Generated code seems not setting DIEANADx, I would try adding to main:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DIENADL |= (1&amp;lt;&amp;lt;5);&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jul 2019 18:08:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12ZVL-ADC-external-trigger/m-p/967137#M16812</guid>
      <dc:creator>kef2</dc:creator>
      <dc:date>2019-07-25T18:08:06Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S12ZVL ADC external trigger</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12ZVL-ADC-external-trigger/m-p/967138#M16813</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Edward,&amp;nbsp;&lt;/P&gt;&lt;P&gt;You were right. PE didn't generate the code for pin setting. But in my code there is next issue apart from of this. After set the input pin, there is needed to set the RSTA bit in the ADCFLWCTL register, and in case when restart mode is used (as in my example)&amp;nbsp; when the end of list is reached, the RSTA bit has to be re-set.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jul 2019 12:45:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12ZVL-ADC-external-trigger/m-p/967138#M16813</guid>
      <dc:creator>lukasz_bittner</dc:creator>
      <dc:date>2019-07-26T12:45:00Z</dc:date>
    </item>
  </channel>
</rss>