<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Re: Device is secure</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Device-is-secure/m-p/963943#M16785</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Hui,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This issue is related to the connection of BDM interface, I can pick up some possible issue:&lt;/P&gt;&lt;P&gt;- The power supply should be 12 V&lt;/P&gt;&lt;P&gt;- Check the orientation of the BDM connector&lt;/P&gt;&lt;P&gt;- Check if the BDM cable is not damaged&lt;/P&gt;&lt;P&gt;- Check if the MCU warms up (If yes, it can be damaged)&lt;/P&gt;&lt;P&gt;- Do you have connected more than one BDM interface?&lt;/P&gt;&lt;P&gt;- You can try to use different USB PORT&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Jun 2019 09:08:36 GMT</pubDate>
    <dc:creator>dianabatrlova</dc:creator>
    <dc:date>2019-06-12T09:08:36Z</dc:date>
    <item>
      <title>Device is secure</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Device-is-secure/m-p/963941#M16783</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I have a&amp;nbsp;Board with S12ZVL&amp;nbsp;MCU embedded in it.when&amp;nbsp;I try to&amp;nbsp;debug a project&amp;nbsp;and use U-Multilink .I'm getting this error "Device is secure .Erase to unsecure"&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/85719i61227ADAA1261E8C/image-size/large?v=v2&amp;amp;px=999" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/85720i020D6D6322D1B178/image-size/large?v=v2&amp;amp;px=999" title="2.png" alt="2.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;How do I solve this issue?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Jun 2019 02:29:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Device-is-secure/m-p/963941#M16783</guid>
      <dc:creator>emma_zhouhui</dc:creator>
      <dc:date>2019-06-10T02:29:56Z</dc:date>
    </item>
    <item>
      <title>Re: Device is secure</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Device-is-secure/m-p/963942#M16784</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please make sure your MCU is powered, as well check if you didn't reverse BDM connector, check BDM cable.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Jun 2019 07:57:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Device-is-secure/m-p/963942#M16784</guid>
      <dc:creator>kef2</dc:creator>
      <dc:date>2019-06-10T07:57:22Z</dc:date>
    </item>
    <item>
      <title>Re: Device is secure</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Device-is-secure/m-p/963943#M16785</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Hui,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This issue is related to the connection of BDM interface, I can pick up some possible issue:&lt;/P&gt;&lt;P&gt;- The power supply should be 12 V&lt;/P&gt;&lt;P&gt;- Check the orientation of the BDM connector&lt;/P&gt;&lt;P&gt;- Check if the BDM cable is not damaged&lt;/P&gt;&lt;P&gt;- Check if the MCU warms up (If yes, it can be damaged)&lt;/P&gt;&lt;P&gt;- Do you have connected more than one BDM interface?&lt;/P&gt;&lt;P&gt;- You can try to use different USB PORT&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jun 2019 09:08:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Device-is-secure/m-p/963943#M16785</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2019-06-12T09:08:36Z</dc:date>
    </item>
  </channel>
</rss>