<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: The issue with SPI function of MC9S12ZVMBA48.</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/The-issue-with-SPI-function-of-MC9S12ZVMBA48/m-p/958270#M16723</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;you are right!&lt;/P&gt;&lt;P&gt;that was problem!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Oct 2019 04:58:27 GMT</pubDate>
    <dc:creator>bluelife85</dc:creator>
    <dc:date>2019-10-11T04:58:27Z</dc:date>
    <item>
      <title>The issue with SPI function of MC9S12ZVMBA48.</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/The-issue-with-SPI-function-of-MC9S12ZVMBA48/m-p/958268#M16721</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a question about the SPI feature of the MC9S12ZVMBA48.&lt;/P&gt;&lt;P&gt;I think I set SPI correctly, but it doesn't do anything at all.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The basis for this is that no signal comes out of the SCK.&lt;/P&gt;&lt;P&gt;I set the MCU as Master of SPI. And I know that when I enter data, the clock comes out on SCK pin by default. However, no clock came out.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is nothing about the SPI pin in the Module Routing Register.&lt;BR /&gt;What should I do?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please review the workspace I attached.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kyungwoo Min.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Sep 2019 04:51:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/The-issue-with-SPI-function-of-MC9S12ZVMBA48/m-p/958268#M16721</guid>
      <dc:creator>bluelife85</dc:creator>
      <dc:date>2019-09-23T04:51:35Z</dc:date>
    </item>
    <item>
      <title>Re: The issue with SPI function of MC9S12ZVMBA48.</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/The-issue-with-SPI-function-of-MC9S12ZVMBA48/m-p/958269#M16722</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/bluelife85@naver.com"&gt;bluelife85@naver.com&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;I'm sorry for the delay.&lt;/P&gt;&lt;P&gt;Could you please read the&amp;nbsp;SPISR register before writing to the&amp;nbsp;SPIDR data register?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Oct 2019 13:40:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/The-issue-with-SPI-function-of-MC9S12ZVMBA48/m-p/958269#M16722</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2019-10-02T13:40:08Z</dc:date>
    </item>
    <item>
      <title>Re: The issue with SPI function of MC9S12ZVMBA48.</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/The-issue-with-SPI-function-of-MC9S12ZVMBA48/m-p/958270#M16723</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;you are right!&lt;/P&gt;&lt;P&gt;that was problem!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Oct 2019 04:58:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/The-issue-with-SPI-function-of-MC9S12ZVMBA48/m-p/958270#M16723</guid>
      <dc:creator>bluelife85</dc:creator>
      <dc:date>2019-10-11T04:58:27Z</dc:date>
    </item>
  </channel>
</rss>