<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 12ZVMC CAN external regulator problem... in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/12ZVMC-CAN-external-regulator-problem/m-p/934496#M16578</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Please check in your design: Recommendation for S12ZVM128 derivatives “On the ZVMC128 a diode is recommended between VDDA and VDDC, whereby the anode is connected to VDDC.”&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;( If we do not have the diodes and board is started up very quickly from a non 0V VDDC (so brown out situation with fast rise time) VDDC can overshoot extremely. On zvmc256 and S12ZVC the diode is internal already present.)&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;At the beginning of the code, for example as a first code in the main function you should mirror your external HW configuration in the internal MCU setup – register CPMUVREGCTL - check it bit by bit.&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;It is not suitable to have enabled both EXTXON and INTXON. If you use/do not use BJT connected to VDDX (see power domain overview and corresponding chapters in the data sheet (I suggest to download the last one) - good to use search keyword “bctl”) then EXTCON,INTCON should be set to 0B10/0b01.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ladislav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Sep 2019 07:01:47 GMT</pubDate>
    <dc:creator>lama</dc:creator>
    <dc:date>2019-09-20T07:01:47Z</dc:date>
    <item>
      <title>12ZVMC CAN external regulator problem...</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/12ZVMC-CAN-external-regulator-problem/m-p/934495#M16577</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have problem with&amp;nbsp;S912ZVMC12F3MKH device. It is BLDC controller with CAN communication and&amp;nbsp; PNP transistor which supplies power to external CAN transceiver. Everything works fine (CAN communication is functional...) for a while, about 3-4 power cycles but then 12ZVMC fails &lt;SPAN&gt;(MCU draws 140mA)&lt;/SPAN&gt;,&amp;nbsp;sometimes together with PNP transistor or CAN transceiver.&lt;/P&gt;&lt;P&gt;&amp;nbsp;Checking the circuit found that BCTLC pin is connected properly, although the base resistor was 5k6 and capacitors had lower value. I did not tried to change it yet.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/89249i9854896F4858F457/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The data sheet&amp;nbsp;says that BCLTC pin should enabled&amp;nbsp;&amp;nbsp;after startup. I am not sure if that was implemented in software.&lt;/P&gt;&lt;P&gt;Is there an example that I can suggest to our software person ?&lt;/P&gt;&lt;P&gt;Ihat else could be reason that external CAN power supply fails after working for a while, at a bench no harsh conditions? I will change base resistor to 1k. Please suggest additional steps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Dragan&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Sep 2019 08:45:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/12ZVMC-CAN-external-regulator-problem/m-p/934495#M16577</guid>
      <dc:creator>draganandric</dc:creator>
      <dc:date>2019-09-17T08:45:16Z</dc:date>
    </item>
    <item>
      <title>Re: 12ZVMC CAN external regulator problem...</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/12ZVMC-CAN-external-regulator-problem/m-p/934496#M16578</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Please check in your design: Recommendation for S12ZVM128 derivatives “On the ZVMC128 a diode is recommended between VDDA and VDDC, whereby the anode is connected to VDDC.”&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;( If we do not have the diodes and board is started up very quickly from a non 0V VDDC (so brown out situation with fast rise time) VDDC can overshoot extremely. On zvmc256 and S12ZVC the diode is internal already present.)&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;At the beginning of the code, for example as a first code in the main function you should mirror your external HW configuration in the internal MCU setup – register CPMUVREGCTL - check it bit by bit.&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;It is not suitable to have enabled both EXTXON and INTXON. If you use/do not use BJT connected to VDDX (see power domain overview and corresponding chapters in the data sheet (I suggest to download the last one) - good to use search keyword “bctl”) then EXTCON,INTCON should be set to 0B10/0b01.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ladislav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Sep 2019 07:01:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/12ZVMC-CAN-external-regulator-problem/m-p/934496#M16578</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2019-09-20T07:01:47Z</dc:date>
    </item>
  </channel>
</rss>