<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic The floating point type was not selected when the project was built. Can it be added in the future? in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/The-floating-point-type-was-not-selected-when-the-project-was/m-p/914714#M16516</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I use code warrior10.7 to built a new project,but &lt;SPAN&gt;forget setting floating point options&lt;/SPAN&gt;&amp;nbsp;,Can it be added in the future?&lt;/P&gt;&lt;P&gt;&amp;nbsp; S912ZVM&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Aug 2019 13:02:52 GMT</pubDate>
    <dc:creator>maxxu</dc:creator>
    <dc:date>2019-08-28T13:02:52Z</dc:date>
    <item>
      <title>The floating point type was not selected when the project was built. Can it be added in the future?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/The-floating-point-type-was-not-selected-when-the-project-was/m-p/914714#M16516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I use code warrior10.7 to built a new project,but &lt;SPAN&gt;forget setting floating point options&lt;/SPAN&gt;&amp;nbsp;,Can it be added in the future?&lt;/P&gt;&lt;P&gt;&amp;nbsp; S912ZVM&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Aug 2019 13:02:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/The-floating-point-type-was-not-selected-when-the-project-was/m-p/914714#M16516</guid>
      <dc:creator>maxxu</dc:creator>
      <dc:date>2019-08-28T13:02:52Z</dc:date>
    </item>
    <item>
      <title>Re: The floating point type was not selected when the project was built. Can it be added in the future?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/The-floating-point-type-was-not-selected-when-the-project-was/m-p/914715#M16517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Max,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can enable floating-point by right click on your project -&amp;gt; Properties and after that select appropriate library&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/83194i2BE35B3E5DB5FA4D/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This question was already discussed in the community, for example, in the link below. I recommend you to read a Note where are described ANSI libraries, it helps you to select the right one.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/message/849209?commentID=849209#comment-849209" title="https://community.nxp.com/message/849209?commentID=849209#comment-849209"&gt;https://community.nxp.com/message/849209?commentID=849209#comment-849209&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Aug 2019 08:07:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/The-floating-point-type-was-not-selected-when-the-project-was/m-p/914715#M16517</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2019-08-30T08:07:38Z</dc:date>
    </item>
  </channel>
</rss>