<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Re: Bootloader CAN for S12Z</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Bootloader-CAN-for-S12Z/m-p/909501#M16489</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;we are very sorry but we are not able to provide you CAN bootloader.&lt;/P&gt;&lt;P&gt;However, principles are the same. The only difference is that data goes via CAN.&lt;/P&gt;&lt;P&gt;We provide an Uart examples because there is simple connection to a PC and there is good amount of UART communication applications which are free.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ladislav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Oct 2019 07:24:01 GMT</pubDate>
    <dc:creator>lama</dc:creator>
    <dc:date>2019-10-23T07:24:01Z</dc:date>
    <item>
      <title>Bootloader CAN for S12Z</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Bootloader-CAN-for-S12Z/m-p/909500#M16488</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm writing a bootloader for a S12ZVC microcontroller for flashing the firmware throught CAN bus. I see that in&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN4723.pdf"&gt;AN4723 - S12Z MagniV Bootloader&lt;/A&gt;&amp;nbsp;Application Note, there is an example of bootloader with SCI protocol. There is an example on CAN protocol too?&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Antonio&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 12 Oct 2019 07:55:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Bootloader-CAN-for-S12Z/m-p/909500#M16488</guid>
      <dc:creator>giacomantonio_n</dc:creator>
      <dc:date>2019-10-12T07:55:12Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader CAN for S12Z</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Bootloader-CAN-for-S12Z/m-p/909501#M16489</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;we are very sorry but we are not able to provide you CAN bootloader.&lt;/P&gt;&lt;P&gt;However, principles are the same. The only difference is that data goes via CAN.&lt;/P&gt;&lt;P&gt;We provide an Uart examples because there is simple connection to a PC and there is good amount of UART communication applications which are free.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ladislav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Oct 2019 07:24:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Bootloader-CAN-for-S12Z/m-p/909501#M16489</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2019-10-23T07:24:01Z</dc:date>
    </item>
  </channel>
</rss>