<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: VDDA on MC9S12XDP512 in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/VDDA-on-MC9S12XDP512/m-p/131974#M1646</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello Michael,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Also bear in mind that the digital signals on the&amp;nbsp;PCB will also be correspondingly smaller, and should result in a lower "noise" level, all other things being equal.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;To minimize noise, the PCB layout should keep the analog traces well separated from any digital traces.&amp;nbsp; If ground traces are used for shielding purposes, these should typically originate directly from the&amp;nbsp;VssA pin.&amp;nbsp; It is also probably a good idea for the buffer circuitry (voltage divider) &amp;nbsp;to &lt;U&gt;reduce&lt;/U&gt; the analog swing to 3 volts&amp;nbsp;maximum, to be located as close to the analog input pins of the MCU as practicable.&amp;nbsp; However, this would not be the case if the "raw" analog signal required amplification.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Oct 2006 08:53:55 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2006-10-04T08:53:55Z</dc:date>
    <item>
      <title>VDDA on MC9S12XDP512</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/VDDA-on-MC9S12XDP512/m-p/131971#M1643</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I am using the MC9S12XDP512.&lt;/DIV&gt;&lt;DIV&gt;VDDR is connected to a 3.3Volts voltage regulator.&lt;/DIV&gt;&lt;DIV&gt;I hoped to connect the VDDA to 5Volts so as to be able to connect to external devices which use 5Volts analog signals.&lt;/DIV&gt;&lt;DIV&gt;However when I connect the 5Volts supply to the VDDA and VRH inputs the VDDR becomes some 4V!&lt;/DIV&gt;&lt;DIV&gt;Is it not allowed to connect the VDDA to a voltage which is higher than VDDR?&lt;/DIV&gt;&lt;DIV&gt;I have searched all over in the datasheets and cannot see anything which states this.&lt;/DIV&gt;&lt;DIV&gt;What is also interesting is that if I leave these pins (VDDA and VRH) unconnected there is a voltave of about 2.68Volts on these pins.&lt;/DIV&gt;&lt;DIV&gt;Can someone explain this behavour please?&amp;nbsp; I am sure that I am missing something&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks a lot&lt;/DIV&gt;&lt;DIV&gt;Michael&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 30 Sep 2006 04:15:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/VDDA-on-MC9S12XDP512/m-p/131971#M1643</guid>
      <dc:creator>mfarr</dc:creator>
      <dc:date>2006-09-30T04:15:38Z</dc:date>
    </item>
    <item>
      <title>Re: VDDA on MC9S12XDP512</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/VDDA-on-MC9S12XDP512/m-p/131972#M1644</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Hi !&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;You probably put yourself in a "&lt;STRONG&gt;current injection&lt;/STRONG&gt;" situation.&lt;/DIV&gt;&lt;DIV&gt;No value anywhere is&amp;nbsp;supposed to stay &lt;EM&gt;&amp;gt;Vdd.&lt;/EM&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;To protect the MCU, you have diodes to Vdd and ground. "&lt;STRONG&gt;Clamp diodes&lt;/STRONG&gt;"&lt;/DIV&gt;&lt;DIV&gt;Therefore once the voltage is above Vdd+0.3 to Vdd+0.6V the diode starts to conduct.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Be careful not to go greater than the injection current specified in the datasheet not to damage the MCU.&lt;/DIV&gt;&lt;DIV&gt;The several voltages you have are for the I/O structures (3.3-5V), for the core itself (CPU and internal logic), the analogue supply and analogue reference.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;There is a AppNote to help you translate levels. &lt;A href="http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&amp;amp;message.id=1161&amp;amp;srch=1" target="_blank"&gt;&lt;STRONG&gt;And also the subject has been discussed on the 8-Bit board&lt;/STRONG&gt;&lt;/A&gt;&lt;STRONG&gt;.&lt;/STRONG&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Cheers,&lt;/DIV&gt;&lt;DIV&gt;Alvin.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;A href="http://www.freescale.com/files/microcontrollers/doc/app_note/AN2433.pdf?srch=1" rel="nofollow" target="_blank"&gt;&lt;STRONG&gt;AN2433 -&lt;/STRONG&gt;&lt;/A&gt; &lt;A href="http://www.freescale.com/files/microcontrollers/doc/app_note/AN2433.pdf?srch=1" rel="nofollow" target="_blank"&gt;&lt;SPAN&gt;&lt;STRONG&gt;5V to 3V Design Considerations&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/A&gt; &lt;STRONG&gt;| pdf&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The move from 5V to 3V technology creates a challenging scenario for system designers. This application note will address the benefits that such a change brings and the design considerations that make the transition as smooth as possible.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Oct 2006 03:35:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/VDDA-on-MC9S12XDP512/m-p/131972#M1644</guid>
      <dc:creator>Nabla69</dc:creator>
      <dc:date>2006-10-02T03:35:05Z</dc:date>
    </item>
    <item>
      <title>Re: VDDA on MC9S12XDP512</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/VDDA-on-MC9S12XDP512/m-p/131973#M1645</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Alvin,&lt;/DIV&gt;&lt;DIV&gt;Thanks for replying to my post.&lt;/DIV&gt;&lt;DIV&gt;So it seems that I have to put level converters between the CPU and my analog inputs.&lt;/DIV&gt;&lt;DIV&gt;I hoped to be able to work at 5Volts.&amp;nbsp; I think with 3 Volts the analog inputs are more subject to noise generated on the PCB itself.&amp;nbsp; A noise of 1mV will now be compared to 3Volts instead of the former 5Volts - that is 1.6 times more!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards&lt;/DIV&gt;&lt;DIV&gt;Michael&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Oct 2006 02:33:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/VDDA-on-MC9S12XDP512/m-p/131973#M1645</guid>
      <dc:creator>mfarr</dc:creator>
      <dc:date>2006-10-04T02:33:14Z</dc:date>
    </item>
    <item>
      <title>Re: VDDA on MC9S12XDP512</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/VDDA-on-MC9S12XDP512/m-p/131974#M1646</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello Michael,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Also bear in mind that the digital signals on the&amp;nbsp;PCB will also be correspondingly smaller, and should result in a lower "noise" level, all other things being equal.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;To minimize noise, the PCB layout should keep the analog traces well separated from any digital traces.&amp;nbsp; If ground traces are used for shielding purposes, these should typically originate directly from the&amp;nbsp;VssA pin.&amp;nbsp; It is also probably a good idea for the buffer circuitry (voltage divider) &amp;nbsp;to &lt;U&gt;reduce&lt;/U&gt; the analog swing to 3 volts&amp;nbsp;maximum, to be located as close to the analog input pins of the MCU as practicable.&amp;nbsp; However, this would not be the case if the "raw" analog signal required amplification.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Oct 2006 08:53:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/VDDA-on-MC9S12XDP512/m-p/131974#M1646</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2006-10-04T08:53:55Z</dc:date>
    </item>
  </channel>
</rss>