<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic freezing some variables when warm reset (reset without powering down) occurs in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/freezing-some-variables-when-warm-reset-reset-without-powering/m-p/898695#M16426</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi every one. I am working on Instrument Cluster which uses MC9s12xhy128 and the firmware is created by codewarrior 5.1 IDE. i have enabled the WDT and i want to hold some variables (like pointer position of panels) if WDT resets the micro-controller. any suggestion?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 May 2019 10:03:31 GMT</pubDate>
    <dc:creator>ma85_bahar</dc:creator>
    <dc:date>2019-05-02T10:03:31Z</dc:date>
    <item>
      <title>freezing some variables when warm reset (reset without powering down) occurs</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/freezing-some-variables-when-warm-reset-reset-without-powering/m-p/898695#M16426</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi every one. I am working on Instrument Cluster which uses MC9s12xhy128 and the firmware is created by codewarrior 5.1 IDE. i have enabled the WDT and i want to hold some variables (like pointer position of panels) if WDT resets the micro-controller. any suggestion?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 May 2019 10:03:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/freezing-some-variables-when-warm-reset-reset-without-powering/m-p/898695#M16426</guid>
      <dc:creator>ma85_bahar</dc:creator>
      <dc:date>2019-05-02T10:03:31Z</dc:date>
    </item>
    <item>
      <title>Re: freezing some variables when warm reset (reset without powering down) occurs</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/freezing-some-variables-when-warm-reset-reset-without-powering/m-p/898696#M16427</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You can divide RAM into segments and use NO_INIT on one of them in the linker file.&lt;/P&gt;&lt;P&gt;From CW5.x help search:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/79849i672A42DAF0A6156B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 May 2019 10:25:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/freezing-some-variables-when-warm-reset-reset-without-powering/m-p/898696#M16427</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2019-05-02T10:25:28Z</dc:date>
    </item>
  </channel>
</rss>