<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How do I find which interrupt is unhandled? in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-do-I-find-which-interrupt-is-unhandled/m-p/884803#M16357</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using S12ZVCA &amp;amp; Codewarrior v11.0.1. The system generated unhandled interrupt sometimes.&lt;/P&gt;&lt;P&gt;How to find out the&amp;nbsp;unhandled interrupt?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/79171i67A45E85217FDCF1/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Aaron&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 07 Apr 2019 09:38:54 GMT</pubDate>
    <dc:creator>aaronlee</dc:creator>
    <dc:date>2019-04-07T09:38:54Z</dc:date>
    <item>
      <title>How do I find which interrupt is unhandled?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-do-I-find-which-interrupt-is-unhandled/m-p/884803#M16357</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using S12ZVCA &amp;amp; Codewarrior v11.0.1. The system generated unhandled interrupt sometimes.&lt;/P&gt;&lt;P&gt;How to find out the&amp;nbsp;unhandled interrupt?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/79171i67A45E85217FDCF1/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Aaron&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 07 Apr 2019 09:38:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-do-I-find-which-interrupt-is-unhandled/m-p/884803#M16357</guid>
      <dc:creator>aaronlee</dc:creator>
      <dc:date>2019-04-07T09:38:54Z</dc:date>
    </item>
    <item>
      <title>Re: How do I find which interrupt is unhandled?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-do-I-find-which-interrupt-is-unhandled/m-p/884804#M16358</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Aaron,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At first, I would like&amp;nbsp;to recommend you to look at the interrupt catcher example code for the S12ZVL,&lt;/P&gt;&lt;P&gt;however, you can use it for the S12ZVC. See link below:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-330312"&gt;https://community.nxp.com/docs/DOC-330312&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using the interrupt table should be able to process all unexpected interrupts.&lt;BR /&gt;Also,&amp;nbsp;Table 1-13. Interrupt Vector Location in RM rev&amp;nbsp;2.0 can be useful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Apr 2019 08:56:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-do-I-find-which-interrupt-is-unhandled/m-p/884804#M16358</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2019-04-08T08:56:28Z</dc:date>
    </item>
  </channel>
</rss>