<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Max voltage can be applied for BLDC in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Max-voltage-can-be-applied-for-BLDC/m-p/878974#M16332</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;MagniV MCUs target 12V automotive applications.&lt;/P&gt;&lt;P&gt;The the following application notes discuss MagniV in 24V and 48V applications.&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN11967.pdf"&gt;AN11967 S12ZVM Family in 48 V Applications&amp;nbsp;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/files-static/microcontrollers/doc/app_note/AN5082.pdf"&gt;AN5082 MagniV in 24V Applications&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Apr 2019 11:24:14 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2019-04-04T11:24:14Z</dc:date>
    <item>
      <title>Max voltage can be applied for BLDC</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Max-voltage-can-be-applied-for-BLDC/m-p/878973#M16331</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello;&lt;/P&gt;&lt;P&gt;i am using MC9s12ZVMx12EVB and using the example for BLDC motor control with the freeMaster (BLDC sensorless) described in AN4704.&lt;/P&gt;&lt;P&gt;the motor runs with no problem, i need to know the max voltage can be applied on the board as i need to operate BLDC with voltage 48V&lt;/P&gt;&lt;P&gt;if the board can operate do i need to change in the software?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Apr 2019 10:19:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Max-voltage-can-be-applied-for-BLDC/m-p/878973#M16331</guid>
      <dc:creator>miko7895</dc:creator>
      <dc:date>2019-04-04T10:19:59Z</dc:date>
    </item>
    <item>
      <title>Re: Max voltage can be applied for BLDC</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Max-voltage-can-be-applied-for-BLDC/m-p/878974#M16332</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;MagniV MCUs target 12V automotive applications.&lt;/P&gt;&lt;P&gt;The the following application notes discuss MagniV in 24V and 48V applications.&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN11967.pdf"&gt;AN11967 S12ZVM Family in 48 V Applications&amp;nbsp;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/files-static/microcontrollers/doc/app_note/AN5082.pdf"&gt;AN5082 MagniV in 24V Applications&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Apr 2019 11:24:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Max-voltage-can-be-applied-for-BLDC/m-p/878974#M16332</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2019-04-04T11:24:14Z</dc:date>
    </item>
  </channel>
</rss>