<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to wakeup the SR12VR with Port L in STOP mode in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-wakeup-the-SR12VR-with-Port-L-in-STOP-mode/m-p/874101#M16275</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using S12VR for STOP mode and wakeup testing. Using a button which is port L&lt;BR /&gt;as wakeup source, and HS0 as pull up, when push the button, Port L will capture a falling&lt;BR /&gt;edge, then Port L will occur a related interrupt which can wakeup S12VR. But seems it can't wakeup S12VR after entering STOP mode. I measured HS0 after STOP mode, seems the voltage is 0.&lt;/P&gt;&lt;P&gt;My question is at this condition, how to wakeup the SR12VR with Port L ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Feb 2019 01:26:35 GMT</pubDate>
    <dc:creator>jeffy_zhou</dc:creator>
    <dc:date>2019-02-20T01:26:35Z</dc:date>
    <item>
      <title>How to wakeup the SR12VR with Port L in STOP mode</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-wakeup-the-SR12VR-with-Port-L-in-STOP-mode/m-p/874101#M16275</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using S12VR for STOP mode and wakeup testing. Using a button which is port L&lt;BR /&gt;as wakeup source, and HS0 as pull up, when push the button, Port L will capture a falling&lt;BR /&gt;edge, then Port L will occur a related interrupt which can wakeup S12VR. But seems it can't wakeup S12VR after entering STOP mode. I measured HS0 after STOP mode, seems the voltage is 0.&lt;/P&gt;&lt;P&gt;My question is at this condition, how to wakeup the SR12VR with Port L ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Feb 2019 01:26:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-wakeup-the-SR12VR-with-Port-L-in-STOP-mode/m-p/874101#M16275</guid>
      <dc:creator>jeffy_zhou</dc:creator>
      <dc:date>2019-02-20T01:26:35Z</dc:date>
    </item>
    <item>
      <title>Re: How to wakeup the SR12VR with Port L in STOP mode</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-wakeup-the-SR12VR-with-Port-L-in-STOP-mode/m-p/874102#M16276</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;How did you configure the Port L pin?&lt;BR /&gt;Please see the below figure, it depends on the STOP/RUN mode.&lt;BR /&gt;The pins have the wakeup capability in Digital input function and it needs to be enabled in the PIEL register.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/75057i13A7A172F74FAF87/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;During stop mode operation the high-side drivers are shut down, i.e. the high-side drivers are&amp;nbsp;disabled and their drivers are turned off. The bits in the data register which control the drivers&amp;nbsp;(HSDRx) are cleared automatically.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Feb 2019 15:22:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-wakeup-the-SR12VR-with-Port-L-in-STOP-mode/m-p/874102#M16276</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2019-02-20T15:22:17Z</dc:date>
    </item>
  </channel>
</rss>