<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: Question Regarding VSUP pin implementation in Magni V</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Question-Regarding-VSUP-pin-implementation-in-Magni-V/m-p/852155#M16125</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kunmit,&lt;/P&gt;&lt;P&gt;The VSUP voltage is divided by 9 (+- 5% max error) and this is what the ADC can measure.&lt;BR /&gt;However, it can’t measure in the whole range of VSUP (Table I-1, #1, S12ZVHY RM), It is limited to 5.5V &amp;lt; VSUP &amp;lt; 29V.&lt;/P&gt;&lt;P&gt;Meaning that if, for example, VSUP = 4V, the ADC result would be higher as if VSUP was 5.5V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Mar 2019 11:20:48 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2019-03-26T11:20:48Z</dc:date>
    <item>
      <title>Question Regarding VSUP pin implementation in Magni V</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Question-Regarding-VSUP-pin-implementation-in-Magni-V/m-p/852154#M16124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;I am using 'MC9S12ZVHY' series MagniV Microcontroller. Need to monitor the Analog voltage range from 0 to 5 V.&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;I am using the VSUP pin&amp;nbsp;for this purpose which can be routed to internal ADC through an Internal Voltage Divider.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;The VSUP pin has following characteristics :&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/67536i23ABC3AB9AE6BFF6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;i Am confused with the above mentioned Condition " 5.5V &amp;lt; VSUP &amp;lt; 29 V" .&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;My Question is:&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Can i use the VSUP pin as internal ADC to Measure analog voltage from 0 to 5V Range?&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Please help me on this issue.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Thanks&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Kunmit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Mar 2019 06:12:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Question-Regarding-VSUP-pin-implementation-in-Magni-V/m-p/852154#M16124</guid>
      <dc:creator>kunmitpatra</dc:creator>
      <dc:date>2019-03-26T06:12:36Z</dc:date>
    </item>
    <item>
      <title>Re: Question Regarding VSUP pin implementation in Magni V</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Question-Regarding-VSUP-pin-implementation-in-Magni-V/m-p/852155#M16125</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kunmit,&lt;/P&gt;&lt;P&gt;The VSUP voltage is divided by 9 (+- 5% max error) and this is what the ADC can measure.&lt;BR /&gt;However, it can’t measure in the whole range of VSUP (Table I-1, #1, S12ZVHY RM), It is limited to 5.5V &amp;lt; VSUP &amp;lt; 29V.&lt;/P&gt;&lt;P&gt;Meaning that if, for example, VSUP = 4V, the ADC result would be higher as if VSUP was 5.5V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Mar 2019 11:20:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Question-Regarding-VSUP-pin-implementation-in-Magni-V/m-p/852155#M16125</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2019-03-26T11:20:48Z</dc:date>
    </item>
  </channel>
</rss>