<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Internal I2C single Byte Read in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Internal-I2C-single-Byte-Read/m-p/852053#M16123</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I don't see the clock of the read byte.&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you disconnect the master from the bus, is the bus hold by the slave low?&lt;/P&gt;&lt;P&gt;Can you share your code?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anyway, you can use the attached example, the S12ZVC MCU has the same IICV3 module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 07 Jan 2019 11:02:12 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2019-01-07T11:02:12Z</dc:date>
    <item>
      <title>Internal I2C single Byte Read</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Internal-I2C-single-Byte-Read/m-p/852052#M16122</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to communicate with FXLS8962 accelerator with S12ZVL32 starter kit.&amp;nbsp;&lt;/P&gt;&lt;P&gt;For drivers i am using the InternalI2C with processor expert.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In order to do operations :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/71351i6EB6CF995E4814A3/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However I am not able to read WHO AM I register 13.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The slave address is 18 whrn SA0 = GND.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As on can see, I send the start, device address with write, receive ACK. then the register to read, THen repeated start and device address with read bit , then i dont receive anything in the I2C bus.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/71399iD5F8147C63F70DF1/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Jan 2019 13:16:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Internal-I2C-single-Byte-Read/m-p/852052#M16122</guid>
      <dc:creator>sarvraj_5</dc:creator>
      <dc:date>2019-01-03T13:16:25Z</dc:date>
    </item>
    <item>
      <title>Re: Internal I2C single Byte Read</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Internal-I2C-single-Byte-Read/m-p/852053#M16123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I don't see the clock of the read byte.&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you disconnect the master from the bus, is the bus hold by the slave low?&lt;/P&gt;&lt;P&gt;Can you share your code?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anyway, you can use the attached example, the S12ZVC MCU has the same IICV3 module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Jan 2019 11:02:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Internal-I2C-single-Byte-Read/m-p/852053#M16123</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2019-01-07T11:02:12Z</dc:date>
    </item>
  </channel>
</rss>