<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Max3050 CAN communication with XEP100 in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Max3050-CAN-communication-with-XEP100/m-p/848557#M16096</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I am working on CAN communication between two XEP100 controllers. I am using MAX3050 CAN IC.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The resistance between CANH and CANL is to be 120 Ohm, but I am getting 167KOhm.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is causing problem in communication, I am getting a dummy data in Rx side.&lt;/P&gt;&lt;P&gt;Please guide me regarding this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Madhura&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 08 Dec 2018 04:34:26 GMT</pubDate>
    <dc:creator>madhura_bhandig</dc:creator>
    <dc:date>2018-12-08T04:34:26Z</dc:date>
    <item>
      <title>Max3050 CAN communication with XEP100</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Max3050-CAN-communication-with-XEP100/m-p/848557#M16096</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I am working on CAN communication between two XEP100 controllers. I am using MAX3050 CAN IC.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The resistance between CANH and CANL is to be 120 Ohm, but I am getting 167KOhm.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is causing problem in communication, I am getting a dummy data in Rx side.&lt;/P&gt;&lt;P&gt;Please guide me regarding this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Madhura&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 08 Dec 2018 04:34:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Max3050-CAN-communication-with-XEP100/m-p/848557#M16096</guid>
      <dc:creator>madhura_bhandig</dc:creator>
      <dc:date>2018-12-08T04:34:26Z</dc:date>
    </item>
    <item>
      <title>Re: Max3050 CAN communication with XEP100</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Max3050-CAN-communication-with-XEP100/m-p/848558#M16097</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm not familiar with&amp;nbsp;MAX3050 but I guess you should add an external 120ohm termination.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Dec 2018 20:10:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Max3050-CAN-communication-with-XEP100/m-p/848558#M16097</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-12-11T20:10:24Z</dc:date>
    </item>
  </channel>
</rss>