<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックMC9S12 CAN bus message transmit only once</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12-CAN-bus-message-transmit-only-once/m-p/847864#M16082</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I did a test with multi-CAN devices, and the S12 transmitted message per 250ms.&lt;/P&gt;&lt;P&gt;I obtained there is no ACK slot on waveform(no one received this message), thus the message was re-send again and again(the interval became only 1ms since message was re-sent&amp;nbsp;nonstop).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just want to know if there is a bit setting in register to ignore ACK or transmit only once, so that i can keep my message cycle time in 250ms.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 19 Nov 2018 03:09:20 GMT</pubDate>
    <dc:creator>peteyo</dc:creator>
    <dc:date>2018-11-19T03:09:20Z</dc:date>
    <item>
      <title>MC9S12 CAN bus message transmit only once</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12-CAN-bus-message-transmit-only-once/m-p/847864#M16082</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I did a test with multi-CAN devices, and the S12 transmitted message per 250ms.&lt;/P&gt;&lt;P&gt;I obtained there is no ACK slot on waveform(no one received this message), thus the message was re-send again and again(the interval became only 1ms since message was re-sent&amp;nbsp;nonstop).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just want to know if there is a bit setting in register to ignore ACK or transmit only once, so that i can keep my message cycle time in 250ms.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Nov 2018 03:09:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12-CAN-bus-message-transmit-only-once/m-p/847864#M16082</guid>
      <dc:creator>peteyo</dc:creator>
      <dc:date>2018-11-19T03:09:20Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S12 CAN bus message transmit only once</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12-CAN-bus-message-transmit-only-once/m-p/847865#M16083</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This is required by the CAN standard.&lt;/P&gt;&lt;P&gt;You can refer to:&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/files/microcontrollers/doc/data_sheet/BCANPSV2.pdf" title="https://www.nxp.com/files/microcontrollers/doc/data_sheet/BCANPSV2.pdf"&gt;https://www.nxp.com/files/microcontrollers/doc/data_sheet/BCANPSV2.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/77619iEC652A73F2E550AA/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Nov 2018 15:00:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12-CAN-bus-message-transmit-only-once/m-p/847865#M16083</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-11-21T15:00:41Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S12 CAN bus message transmit only once</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12-CAN-bus-message-transmit-only-once/m-p/847866#M16084</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found a setting as below and it seems like this setting could stop retransmission even there is an error or non-ACK situation. If I schedule a 250ms cycle time transmission with setting these bits high and&amp;nbsp; then remove other devices on the bus(only one device on the bus), the CAN bus signals would keep in 250ms.(sometimes loss but no retransmission)&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/77857i3C3A6606FB8073F0/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Nov 2018 02:47:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MC9S12-CAN-bus-message-transmit-only-once/m-p/847866#M16084</guid>
      <dc:creator>peteyo</dc:creator>
      <dc:date>2018-11-22T02:47:02Z</dc:date>
    </item>
  </channel>
</rss>