<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic xgate interrupts configuration error in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/xgate-interrupts-configuration-error/m-p/845994#M16067</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi team, we are using MSCAN driver (CAN0). when there is a rx interrupt to CAN0 it should needs to handle by XGATE (not the cpu). can you pls help us how to do that . we configure CAN0 wake-up,CAN0 errors,CAN0 receive, CAN0 transmit as CanTxInterrupt_0, /* 0xFFB0 MSCAN 0 transmit */ CanRxInterrupt_0, /* 0xFFB2 MSCAN 0 receive */ CanErrorInterrupt_0, /* 0xFFB4 MSCAN 0 errors */ CanWakeUpInterrupt_0, /* 0xFFB6 MSCAN 0 wake-up */ setprio(0x58, 0x06); // CAN0 transmit - setprio(0x59, 0x07); // CAN0 receive - Highest setprio(0x5A, 0x02); // CAN0 errors - Low setprio(0x5B, 0x05); // CAN0 wake-up - setprio(0x3D, 0x01); // PTI0 UNDEFD,//{(void (*)(void))CanXGateRxInterrupt, &amp;amp;CanXGateArgs[0]}, /* 0x59 MSCAN 0 receive */ the above interrupt need to handle by XGATE . pls help what needs to be done&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 Aug 2018 10:09:07 GMT</pubDate>
    <dc:creator>krishnan64</dc:creator>
    <dc:date>2018-08-30T10:09:07Z</dc:date>
    <item>
      <title>xgate interrupts configuration error</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/xgate-interrupts-configuration-error/m-p/845994#M16067</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi team, we are using MSCAN driver (CAN0). when there is a rx interrupt to CAN0 it should needs to handle by XGATE (not the cpu). can you pls help us how to do that . we configure CAN0 wake-up,CAN0 errors,CAN0 receive, CAN0 transmit as CanTxInterrupt_0, /* 0xFFB0 MSCAN 0 transmit */ CanRxInterrupt_0, /* 0xFFB2 MSCAN 0 receive */ CanErrorInterrupt_0, /* 0xFFB4 MSCAN 0 errors */ CanWakeUpInterrupt_0, /* 0xFFB6 MSCAN 0 wake-up */ setprio(0x58, 0x06); // CAN0 transmit - setprio(0x59, 0x07); // CAN0 receive - Highest setprio(0x5A, 0x02); // CAN0 errors - Low setprio(0x5B, 0x05); // CAN0 wake-up - setprio(0x3D, 0x01); // PTI0 UNDEFD,//{(void (*)(void))CanXGateRxInterrupt, &amp;amp;CanXGateArgs[0]}, /* 0x59 MSCAN 0 receive */ the above interrupt need to handle by XGATE . pls help what needs to be done&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Aug 2018 10:09:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/xgate-interrupts-configuration-error/m-p/845994#M16067</guid>
      <dc:creator>krishnan64</dc:creator>
      <dc:date>2018-08-30T10:09:07Z</dc:date>
    </item>
  </channel>
</rss>