<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: G48 Mass production</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/G48-Mass-production/m-p/843227#M16029</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gary Guo,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;On the MCU is available Program Once Field. It is a part of Flash IFR which can be&lt;BR /&gt;used to store non-volatile data.&lt;BR /&gt;The global memory from 0x0_4000 is accessible when we set NVMRES bit&lt;BR /&gt;(MMCCTL1=0x01;) at PPAGE 0x01 and memory window 0x8000~0xBFFF.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See&amp;nbsp;Table 24-5. Program IFR Fields in the &lt;A href="https://www.nxp.com/docs/en/data-sheet/MC9S12GRMV1.pdf"&gt;reference manual&lt;/A&gt;.&amp;nbsp;&lt;BR /&gt;Programming the own serial number is possible into Program Once Field - 64B&lt;BR /&gt;at global address 0x0_40C0 – 0x0_40FF.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The additional useful information you can find in this thread:&lt;BR /&gt; &lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/message/869910?commentID=869910#comment-869910" title="https://community.nxp.com/message/869910?commentID=869910#comment-869910"&gt;https://community.nxp.com/message/869910?commentID=869910#comment-869910&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Jul 2018 07:51:28 GMT</pubDate>
    <dc:creator>dianabatrlova</dc:creator>
    <dc:date>2018-07-12T07:51:28Z</dc:date>
    <item>
      <title>G48 Mass production</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/G48-Mass-production/m-p/843226#M16028</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;When the factory burns G48, it needs to write a ID number in each flash of MCU, ID can be incremented. What kind of recorder can be used to achieve it?&lt;/SPAN&gt;&lt;SPAN&gt; How do you realize it?&lt;/SPAN&gt;&lt;SPAN&gt; Thank you&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jul 2018 06:43:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/G48-Mass-production/m-p/843226#M16028</guid>
      <dc:creator>garyws</dc:creator>
      <dc:date>2018-07-03T06:43:27Z</dc:date>
    </item>
    <item>
      <title>Re: G48 Mass production</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/G48-Mass-production/m-p/843227#M16029</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gary Guo,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;On the MCU is available Program Once Field. It is a part of Flash IFR which can be&lt;BR /&gt;used to store non-volatile data.&lt;BR /&gt;The global memory from 0x0_4000 is accessible when we set NVMRES bit&lt;BR /&gt;(MMCCTL1=0x01;) at PPAGE 0x01 and memory window 0x8000~0xBFFF.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See&amp;nbsp;Table 24-5. Program IFR Fields in the &lt;A href="https://www.nxp.com/docs/en/data-sheet/MC9S12GRMV1.pdf"&gt;reference manual&lt;/A&gt;.&amp;nbsp;&lt;BR /&gt;Programming the own serial number is possible into Program Once Field - 64B&lt;BR /&gt;at global address 0x0_40C0 – 0x0_40FF.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The additional useful information you can find in this thread:&lt;BR /&gt; &lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/message/869910?commentID=869910#comment-869910" title="https://community.nxp.com/message/869910?commentID=869910#comment-869910"&gt;https://community.nxp.com/message/869910?commentID=869910#comment-869910&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jul 2018 07:51:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/G48-Mass-production/m-p/843227#M16029</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2018-07-12T07:51:28Z</dc:date>
    </item>
  </channel>
</rss>