<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Re: Xgate on Flash</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Xgate-on-Flash/m-p/131724#M1601</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;XGATE has access to about 30k of flash and you can use this for whatever purpose you want including code space.&lt;/DIV&gt;&lt;DIV&gt;Be aware that XGATE will run at half the speed when fetching code from flash (i.e. same bus speed as the CPU - 40MHz max.) and this is the reason that RAM is the primary recommendation. Essentially flash is slow compared to RAM.&lt;/DIV&gt;&lt;DIV&gt;To place XGATE code in RAM you define the appropriate code segment in the linker file and the linker will place the code where you want it to be.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Apr 2007 19:06:00 GMT</pubDate>
    <dc:creator>Steve</dc:creator>
    <dc:date>2007-04-25T19:06:00Z</dc:date>
    <item>
      <title>Xgate on Flash</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Xgate-on-Flash/m-p/131723#M1600</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm working with mc9s12xdp512 16-bit proccessor. This MCU has Xgate co-processor. Xgate is a great idea for the purpouse of my application but I have some questions that, perphaps, you can resolve.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is it possible to execute Xgate code from Flash or is it a must the code was executed from RAM?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ruben&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Apr 2007 15:37:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Xgate-on-Flash/m-p/131723#M1600</guid>
      <dc:creator>RubenCG</dc:creator>
      <dc:date>2007-04-25T15:37:49Z</dc:date>
    </item>
    <item>
      <title>Re: Xgate on Flash</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Xgate-on-Flash/m-p/131724#M1601</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;XGATE has access to about 30k of flash and you can use this for whatever purpose you want including code space.&lt;/DIV&gt;&lt;DIV&gt;Be aware that XGATE will run at half the speed when fetching code from flash (i.e. same bus speed as the CPU - 40MHz max.) and this is the reason that RAM is the primary recommendation. Essentially flash is slow compared to RAM.&lt;/DIV&gt;&lt;DIV&gt;To place XGATE code in RAM you define the appropriate code segment in the linker file and the linker will place the code where you want it to be.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Apr 2007 19:06:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Xgate-on-Flash/m-p/131724#M1601</guid>
      <dc:creator>Steve</dc:creator>
      <dc:date>2007-04-25T19:06:00Z</dc:date>
    </item>
    <item>
      <title>Re: Xgate on Flash</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Xgate-on-Flash/m-p/131725#M1602</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thank you Steve for your quickly answer. Now I know that I have the two possibilities, probably I'll use the RAM.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Apr 2007 20:18:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Xgate-on-Flash/m-p/131725#M1602</guid>
      <dc:creator>RubenCG</dc:creator>
      <dc:date>2007-04-25T20:18:10Z</dc:date>
    </item>
  </channel>
</rss>