<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: BDM debugging (step over) speed.</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/BDM-debugging-step-over-speed/m-p/833546#M15973</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;There is an option to set the CLKSW bit in the CW.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/69205iFEF0933457019A06/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/69259i360663139291830B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/69300iCE69276DD8982441/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Sep 2018 13:38:27 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2018-09-19T13:38:27Z</dc:date>
    <item>
      <title>BDM debugging (step over) speed.</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/BDM-debugging-step-over-speed/m-p/833544#M15971</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;Am using codewarrior 5.1/5.2 and mc9s12xeq512 controller.&lt;BR /&gt;The borad has a crystal of 16MHz and PLL of 50MHz.&lt;BR /&gt;I have a problem with the step over speed.&lt;BR /&gt;It takes from few milisecond to 4 seconds.&lt;BR /&gt;Most of the times the step over speed is about 1.5 second.&lt;BR /&gt;Of Course the complexity of c line have effect on step over speed, but with 50MHz bus clock, the 1.5 seconds and the 4 seconds of step over is way to long (even PIC16Fxxx is faster).&lt;BR /&gt;When I disable the PLL, the clock bus is only 8MHz, but there is no noticable change of the debugging speed. &lt;BR /&gt;This tells me that BDM uses the crystal oscillator and not PLL.&lt;/P&gt;&lt;P&gt;The CLKSW bit of BDMSTS, controls which clock the BDM operates with, and it is only writable from a hardware BDM command.&lt;BR /&gt;As far as understand, if PLLSEL=1 and CLKSW=1, the BDM Clock Source, dependent on the PLL.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone know how can I set CLKSW, so the BDM will work with the PLL.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Sep 2018 14:01:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/BDM-debugging-step-over-speed/m-p/833544#M15971</guid>
      <dc:creator>Eric_t</dc:creator>
      <dc:date>2018-09-17T14:01:20Z</dc:date>
    </item>
    <item>
      <title>Re: BDM debugging (step over) speed.</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/BDM-debugging-step-over-speed/m-p/833545#M15972</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I forgot to mention that I used pemicro multilink universal FX for debugging.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Sep 2018 14:04:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/BDM-debugging-step-over-speed/m-p/833545#M15972</guid>
      <dc:creator>Eric_t</dc:creator>
      <dc:date>2018-09-17T14:04:14Z</dc:date>
    </item>
    <item>
      <title>Re: BDM debugging (step over) speed.</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/BDM-debugging-step-over-speed/m-p/833546#M15973</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;There is an option to set the CLKSW bit in the CW.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/69205iFEF0933457019A06/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/69259i360663139291830B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/69300iCE69276DD8982441/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Sep 2018 13:38:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/BDM-debugging-step-over-speed/m-p/833546#M15973</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-09-19T13:38:27Z</dc:date>
    </item>
  </channel>
</rss>