<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 INPUT CAPTURE</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/INPUT-CAPTURE/m-p/829129#M15951</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Iam using S12zvml31 controller for sensorless commutation for bldc motor control. I configured TIM0 channel 0 and channel 3 as output compare mode for sensorless algorithm. Now I want to measure external pwm pulse through input capture, in which pin I have to connect that pwm signal. And how to use that TIM0?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Kaarthi.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Jun 2018 06:22:25 GMT</pubDate>
    <dc:creator>kaarthichandras</dc:creator>
    <dc:date>2018-06-28T06:22:25Z</dc:date>
    <item>
      <title>INPUT CAPTURE</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/INPUT-CAPTURE/m-p/829129#M15951</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Iam using S12zvml31 controller for sensorless commutation for bldc motor control. I configured TIM0 channel 0 and channel 3 as output compare mode for sensorless algorithm. Now I want to measure external pwm pulse through input capture, in which pin I have to connect that pwm signal. And how to use that TIM0?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Kaarthi.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jun 2018 06:22:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/INPUT-CAPTURE/m-p/829129#M15951</guid>
      <dc:creator>kaarthichandras</dc:creator>
      <dc:date>2018-06-28T06:22:25Z</dc:date>
    </item>
    <item>
      <title>Re: INPUT CAPTURE</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/INPUT-CAPTURE/m-p/829130#M15952</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You can refer to&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-332554"&gt;S12ZVL-TIM-FrequencyMeasurement-V1_0-CW106-TIC-EXAMPLE&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It can be modified for&amp;nbsp;pulse width measurements.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jul 2018 12:12:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/INPUT-CAPTURE/m-p/829130#M15952</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-07-04T12:12:13Z</dc:date>
    </item>
  </channel>
</rss>