<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: LOW-POWER MODE</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/LOW-POWER-MODE/m-p/825663#M15916</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;To enter Stop or Wait mode use STOP or WAIT instruction.&lt;BR /&gt;The stop instruction is enabled if S control bit is cleared in the CCR core register.&lt;/P&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;asm ANDCC #0x7F; // Clear S bit
asm STOP;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // MCU STOP mode‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;For more information, please refer to &lt;A href="https://www.nxp.com/docs/en/reference-manual/S12ZCPU_RM_V1.pdf" rel="nofollow noopener noreferrer" target="_blank"&gt;CPU S12Z RM&lt;/A&gt;.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Depending on the PSTP, OSCE bits, the MCU can enter either Full Stop mode or Pseudo Stop mode (Section 8.1.2.3, S12ZVC RM rev.1.9).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Every I-bit maskable interrupt is capable to wake up from Stop or Wait mode provided the peripheral that triggers the interrupt is active in the low power mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Nov 2018 11:27:10 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2018-11-13T11:27:10Z</dc:date>
    <item>
      <title>LOW-POWER MODE</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/LOW-POWER-MODE/m-p/825662#M15915</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; I am using S12ZVML31. How can I enter and quit the wait/stop&amp;nbsp; mode? Any examples?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Nov 2018 03:57:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/LOW-POWER-MODE/m-p/825662#M15915</guid>
      <dc:creator>frankkong</dc:creator>
      <dc:date>2018-11-12T03:57:29Z</dc:date>
    </item>
    <item>
      <title>Re: LOW-POWER MODE</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/LOW-POWER-MODE/m-p/825663#M15916</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;To enter Stop or Wait mode use STOP or WAIT instruction.&lt;BR /&gt;The stop instruction is enabled if S control bit is cleared in the CCR core register.&lt;/P&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;asm ANDCC #0x7F; // Clear S bit
asm STOP;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // MCU STOP mode‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;For more information, please refer to &lt;A href="https://www.nxp.com/docs/en/reference-manual/S12ZCPU_RM_V1.pdf" rel="nofollow noopener noreferrer" target="_blank"&gt;CPU S12Z RM&lt;/A&gt;.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Depending on the PSTP, OSCE bits, the MCU can enter either Full Stop mode or Pseudo Stop mode (Section 8.1.2.3, S12ZVC RM rev.1.9).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Every I-bit maskable interrupt is capable to wake up from Stop or Wait mode provided the peripheral that triggers the interrupt is active in the low power mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Nov 2018 11:27:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/LOW-POWER-MODE/m-p/825663#M15916</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-11-13T11:27:10Z</dc:date>
    </item>
    <item>
      <title>Re: LOW-POWER MODE</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/LOW-POWER-MODE/m-p/825664#M15917</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Daniel, it works.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Nov 2018 08:03:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/LOW-POWER-MODE/m-p/825664#M15917</guid>
      <dc:creator>frankkong</dc:creator>
      <dc:date>2018-11-14T08:03:30Z</dc:date>
    </item>
  </channel>
</rss>