<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Difference between samples with MTRCKTSBNZVM128 in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Difference-between-samples-with-MTRCKTSBNZVM128/m-p/815678#M15837</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying motor control with MTRCKTSBNZVM128.&lt;/P&gt;&lt;P&gt;I want someone to answer my question.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the samples MTRCKTSBNZVM128_HALL_CW11 and MTRCKTSBNZVM128_SENSORLESS_CW10.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As shown in the graph below, HALL (1) has larger current consumption than SENSORLESS.&lt;/P&gt;&lt;P&gt;The horizontal axis is the number of revolutions [rpm], and the vertical axis is the current [A].&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/70239i3C21A667B43BD402/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, when you try at a certain time, it is equivalent to SENSORLESS like HALL (2).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I confirmed the source code, but I think both are 120 degree conduction, not vector control.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have not changed the NXP kit at all.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a possibility that the HALL sample behaves like SENSORLESS under some conditions?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd like to receive advice.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Dec 2018 05:32:59 GMT</pubDate>
    <dc:creator>hiro2hiro</dc:creator>
    <dc:date>2018-12-20T05:32:59Z</dc:date>
    <item>
      <title>Difference between samples with MTRCKTSBNZVM128</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Difference-between-samples-with-MTRCKTSBNZVM128/m-p/815678#M15837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying motor control with MTRCKTSBNZVM128.&lt;/P&gt;&lt;P&gt;I want someone to answer my question.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the samples MTRCKTSBNZVM128_HALL_CW11 and MTRCKTSBNZVM128_SENSORLESS_CW10.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As shown in the graph below, HALL (1) has larger current consumption than SENSORLESS.&lt;/P&gt;&lt;P&gt;The horizontal axis is the number of revolutions [rpm], and the vertical axis is the current [A].&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/70239i3C21A667B43BD402/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, when you try at a certain time, it is equivalent to SENSORLESS like HALL (2).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I confirmed the source code, but I think both are 120 degree conduction, not vector control.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have not changed the NXP kit at all.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a possibility that the HALL sample behaves like SENSORLESS under some conditions?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd like to receive advice.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Dec 2018 05:32:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Difference-between-samples-with-MTRCKTSBNZVM128/m-p/815678#M15837</guid>
      <dc:creator>hiro2hiro</dc:creator>
      <dc:date>2018-12-20T05:32:59Z</dc:date>
    </item>
  </channel>
</rss>