<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S12ZVL32 STOP mode accident in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL32-STOP-mode-accident/m-p/812197#M15818</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Yes, only the two instructions are required to put the MCU into Stop Mode.&lt;/P&gt;&lt;P&gt;It seems like the Timer is the wake-up source. Because if there is a pending interrupt while the STOP instruction is being executed, it will prevent the MCU from entering the Stop mode.&lt;/P&gt;&lt;P&gt;Is there a problem disabling the timer interrupt in your application?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Sep 2018 18:29:01 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2018-09-11T18:29:01Z</dc:date>
    <item>
      <title>S12ZVL32 STOP mode accident</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL32-STOP-mode-accident/m-p/812196#M15817</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;the MCU work well most of the time but sometimes the amount of current consumed is about 10Ma after receive LIN sleep command (0x3c),it is still in normal mode by monitoring bus output,then if i send LIN sleep command again,MCU will go sleep mode well .&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I am using S12ZVL32.&lt;BR /&gt;I put the MCU in full stop mode by LIN (0x3c) and wake up by input active interrupt;&lt;BR /&gt;I judged the mode by current measurement and bus output(ECLKCTL_NECLK=0).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;problem 1:__asm(ANDCC #0x7F); __asm(STOP); // Are these two instructions going to make the MCU enter the stop mode without any other prerequisites?&lt;/P&gt;&lt;P&gt;problem 2:I have two guesses, enter stop mode failure or break out of stop mode through the default interrupts of MCU systems which I not configurate in the programm.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Something incomprehensible has happend when I disable the TIMER interrupt before STOP instruction,MCU always work successfully.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;//Experiments show that ecu_enter_sleep_mode() will be always executed after receive sleep command LIN(0x3c)&lt;BR /&gt;void ecu_enter_sleep_mode(void)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; SCI0ASR1_RXEDGIF = 1;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; SCI0ACR1_RXEDGIE = 1; &lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;//TIM0TIE = 0x00;//timer interrupt is enabled all the time.if i disable the timer interrupt during stop mode,MCU always &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;work well. &lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;port_set_low_power_mode(); &lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; cpu_set_stop_mode();//#define cpu_set_stop_mode() { __asm(ANDCC #0x7F); __asm(STOP); } &lt;BR /&gt;}&lt;BR /&gt;void wake_up_ecu(void)&lt;BR /&gt;{ &lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;// TIM0TIE = 0x21;//the instruction should be added if disabled before. &lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;port_init(); &lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;// Suppose cpu_set_stop_mode() let the MCU go into stop mode.&lt;BR /&gt;// Experiments show that When an exception occurs ,the MCU break out of stop mode not through SCI0 interrupt program &lt;BR /&gt;// I'm sure that I only use TIMER interrupt and input active interrupt.Could it be the system's default interrupt program?&lt;BR /&gt;void sci0_isr_handler(void)&lt;BR /&gt;{&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;if (SCI0ASR1_RXEDGIF == 1 &amp;amp;&amp;amp; SCI0ACR1_RXEDGIE == 1) /* An active edge on the receive input has occurred */&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;{&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;SCI0ACR1_RXEDGIE = 0;&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;SCI0ASR1_RXEDGIF = 1; &lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;}&lt;BR /&gt;}&lt;BR /&gt;It is a long time since I am trying to fix this problem and now I have no other ideas to fix it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Sep 2018 05:05:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL32-STOP-mode-accident/m-p/812196#M15817</guid>
      <dc:creator>fanziyu</dc:creator>
      <dc:date>2018-09-11T05:05:05Z</dc:date>
    </item>
    <item>
      <title>Re: S12ZVL32 STOP mode accident</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL32-STOP-mode-accident/m-p/812197#M15818</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Yes, only the two instructions are required to put the MCU into Stop Mode.&lt;/P&gt;&lt;P&gt;It seems like the Timer is the wake-up source. Because if there is a pending interrupt while the STOP instruction is being executed, it will prevent the MCU from entering the Stop mode.&lt;/P&gt;&lt;P&gt;Is there a problem disabling the timer interrupt in your application?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Sep 2018 18:29:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL32-STOP-mode-accident/m-p/812197#M15818</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-09-11T18:29:01Z</dc:date>
    </item>
    <item>
      <title>Re: S12ZVL32 STOP mode accident</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL32-STOP-mode-accident/m-p/812198#M15819</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for your reply.There is no problem disabling the timer interrupt in the application.&lt;/P&gt;&lt;P&gt;But there is still a problem confused me that :&amp;nbsp;&amp;nbsp;&amp;nbsp;Do you mean when the&amp;nbsp;__asm(STOP) is being executed suddenly&amp;nbsp; an interrupt&amp;nbsp;generated,then MCU go to stop mode failed?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;STOP process&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;//&lt;/SPAN&gt;An interrupt between 1 and 6 will cause the STOP instruction to fail ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;1:（SP）-$0002 SP;&lt;BR /&gt;2:（SP）-$0002 SP;&lt;BR /&gt;3:（SP）-$0002 SP;&lt;BR /&gt;4:（SP）-$0002 SP;&lt;BR /&gt;5:（SP）-$0001 SP;&lt;BR /&gt;6: STOP ALL Clocks&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ANDCC Description:&amp;nbsp;&lt;/P&gt;&lt;P&gt;if the I mask bit is cleared,there is a 1-cycle delay before the system allows interrupt requests .This prevents interrupts from occurring between instructions in the sequences CLI,WAI and STOP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have used below programm ,it has the same problem that sometimes the&amp;nbsp;the amount of current consumed is about 10Ma after receive LIN sleep command (0x3c)&lt;/P&gt;&lt;P&gt;void ecu_enter_sleep_mode(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;SCI0ACR1_RXEDGIE = 1; /* Enable receive input active edge interrupt */&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;SCI0ASR1_RXEDGIF = 1;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;//TIM0TIE = 0x00;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;//timer interrupt is enabled all the time.if i disable the timer interrupt during stop &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;mode,MCU always work well.&amp;nbsp;&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;port_set_low_power_mode(); &lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;DisableInterrupts; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;//from 0N22G ERRATA Shutdown sequence is not interruptible until STOP;&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;ADC0_stop_current_workaround();//from 0N22G ERRATA&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;ADC0CTL_0 = 0X00;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; //ADC is disabled&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;cpu_set_stop_mode(); &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;//#define cpu_set_stop_mode() { __asm(ANDCC #0x6F); __asm(STOP); }&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Sep 2018 05:17:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL32-STOP-mode-accident/m-p/812198#M15819</guid>
      <dc:creator>fanziyu</dc:creator>
      <dc:date>2018-09-12T05:17:18Z</dc:date>
    </item>
    <item>
      <title>Re: S12ZVL32 STOP mode accident</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL32-STOP-mode-accident/m-p/812199#M15820</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The code&amp;nbsp;masks interrupts, disables ADC and clears the interrupt mask again. It the Timer triggers during the ADC operation, the interrupt becomes pending. Once I bit gets cleared, the Stop instruction will be executed but because there is a pending interrupt, it will wake it up.&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can place a few NOP instructions after CLI and before STOP.&amp;nbsp;&lt;/P&gt;&lt;P&gt;If there is a pending interrupt, it will be served before the MCU enters Stop Mode.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But I would disable the Timer interrupt anyway, so that it can't trigger during the STOP instruction execution before clocks are disabled.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Sep 2018 10:49:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL32-STOP-mode-accident/m-p/812199#M15820</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-09-12T10:49:01Z</dc:date>
    </item>
    <item>
      <title>Re: S12ZVL32 STOP mode accident</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL32-STOP-mode-accident/m-p/812200#M15821</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;your&amp;nbsp; support!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;thanks and regards&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;wenbin&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Sep 2018 12:37:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL32-STOP-mode-accident/m-p/812200#M15821</guid>
      <dc:creator>fanziyu</dc:creator>
      <dc:date>2018-09-12T12:37:07Z</dc:date>
    </item>
  </channel>
</rss>