<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: Interrupt Soure</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Interrupt-Soure/m-p/792131#M15622</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You can use an interrupt catcher like the one attached.&lt;/P&gt;&lt;P&gt;The variable 'number_of_ISR' will then identify the vector.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Sep 2018 08:11:10 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2018-09-25T08:11:10Z</dc:date>
    <item>
      <title>Interrupt Soure</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Interrupt-Soure/m-p/792130#M15621</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;With the 9S12XE512 we configure all unused vectors to point to a dummy handler that then throws an exception to halt the code.&lt;/P&gt;&lt;P&gt;I have the situation where this trap function is being called periodically but I can not figure out which interrupt/vector is being called.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I place a break point in my interrupt handler is there any way to determine that vector address that caused the call?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Sep 2018 18:46:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Interrupt-Soure/m-p/792130#M15621</guid>
      <dc:creator>shawnlammers</dc:creator>
      <dc:date>2018-09-24T18:46:52Z</dc:date>
    </item>
    <item>
      <title>Re: Interrupt Soure</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Interrupt-Soure/m-p/792131#M15622</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You can use an interrupt catcher like the one attached.&lt;/P&gt;&lt;P&gt;The variable 'number_of_ISR' will then identify the vector.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Sep 2018 08:11:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Interrupt-Soure/m-p/792131#M15622</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-09-25T08:11:10Z</dc:date>
    </item>
  </channel>
</rss>