<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to Read iic for the S12G64? in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-Read-iic-for-the-S12G64/m-p/775806#M15457</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to read Register of&amp;nbsp;&amp;nbsp;MAX9288 ,but i face to difficulty. I has been read value success.but the reasult is zero .&lt;/P&gt;&lt;P&gt;please tell me reason,thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;add: I was read register&amp;nbsp; for the&amp;nbsp;&amp;nbsp;slave address is 0x90.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for example:&lt;/P&gt;&lt;P&gt;byte IIC_9288_RecvBlock_Test(uint8_t addr,void* Ptr,word Siz,word *Rcv)&lt;BR /&gt;{&lt;BR /&gt; word I;&lt;BR /&gt; bool Acknowledge;&lt;BR /&gt; word Trial;&lt;/P&gt;&lt;P&gt;*Rcv = 0U;&lt;BR /&gt; Trial = TRIALS;&lt;BR /&gt; do {&lt;BR /&gt; Inhr1_SetDir((bool)INPUT); /* SDA HIGH - START SETUP */&lt;BR /&gt; Inhr2_SetDir((bool)INPUT); /* CLOCK HIGH PULSE */&lt;BR /&gt; Delay(); /* CLOCK HIGH PULSE + BUS FREE TIME */&lt;BR /&gt; Inhr1_SetDir((bool)OUTPUT);&lt;BR /&gt; Inhr1_ClrVal(); /* START CONDITION */&lt;BR /&gt; Delay(); /* START HOLD TIME */&lt;BR /&gt; Inhr2_SetDir((bool)OUTPUT);&lt;BR /&gt; Inhr2_ClrVal(); /* CLOCK LOW PULSE */&lt;BR /&gt; Delay();&lt;BR /&gt; Write((byte)(addr + READ));&lt;BR /&gt; Acknowledge = GetAck();&lt;BR /&gt; --Trial;&lt;BR /&gt; } &lt;BR /&gt; while((Trial != 0U) &amp;amp;&amp;amp; Acknowledge);&lt;BR /&gt; &lt;BR /&gt; if(Acknowledge) &lt;BR /&gt; {&lt;BR /&gt; IIC_9288_OnNACK();&lt;BR /&gt; Inhr2_SetDir((bool)OUTPUT);&lt;BR /&gt; Inhr2_ClrVal(); /* CLOCK LOW PULSE */&lt;BR /&gt; InternalStop();&lt;BR /&gt; return ERR_BUSY;&lt;BR /&gt; }&lt;BR /&gt; else &lt;BR /&gt; {&lt;BR /&gt; Inhr2_SetDir((bool)OUTPUT);&lt;BR /&gt; Inhr2_ClrVal(); /* CLOCK LOW PULSE */&lt;BR /&gt; Delay();&lt;BR /&gt; }&lt;BR /&gt; &lt;BR /&gt; for (I = 0U; I &amp;lt; Siz; I++)&lt;BR /&gt; {&lt;BR /&gt; *((byte *) Ptr + I) = Read();&lt;BR /&gt; IIC_9288_OnRxChar();&lt;BR /&gt; if (I == (Siz - 1U)) &lt;BR /&gt; {&lt;BR /&gt; SetAck((bool)NOACK);&lt;BR /&gt; }&lt;BR /&gt; else&lt;BR /&gt; {&lt;BR /&gt; SetAck((bool)ACK);&lt;BR /&gt; }&lt;BR /&gt; ++(*Rcv);&lt;BR /&gt; }&lt;BR /&gt; return ERR_OK;&lt;BR /&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Feb 2018 02:38:37 GMT</pubDate>
    <dc:creator>yanlaidong</dc:creator>
    <dc:date>2018-02-01T02:38:37Z</dc:date>
    <item>
      <title>How to Read iic for the S12G64?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-Read-iic-for-the-S12G64/m-p/775806#M15457</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to read Register of&amp;nbsp;&amp;nbsp;MAX9288 ,but i face to difficulty. I has been read value success.but the reasult is zero .&lt;/P&gt;&lt;P&gt;please tell me reason,thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;add: I was read register&amp;nbsp; for the&amp;nbsp;&amp;nbsp;slave address is 0x90.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for example:&lt;/P&gt;&lt;P&gt;byte IIC_9288_RecvBlock_Test(uint8_t addr,void* Ptr,word Siz,word *Rcv)&lt;BR /&gt;{&lt;BR /&gt; word I;&lt;BR /&gt; bool Acknowledge;&lt;BR /&gt; word Trial;&lt;/P&gt;&lt;P&gt;*Rcv = 0U;&lt;BR /&gt; Trial = TRIALS;&lt;BR /&gt; do {&lt;BR /&gt; Inhr1_SetDir((bool)INPUT); /* SDA HIGH - START SETUP */&lt;BR /&gt; Inhr2_SetDir((bool)INPUT); /* CLOCK HIGH PULSE */&lt;BR /&gt; Delay(); /* CLOCK HIGH PULSE + BUS FREE TIME */&lt;BR /&gt; Inhr1_SetDir((bool)OUTPUT);&lt;BR /&gt; Inhr1_ClrVal(); /* START CONDITION */&lt;BR /&gt; Delay(); /* START HOLD TIME */&lt;BR /&gt; Inhr2_SetDir((bool)OUTPUT);&lt;BR /&gt; Inhr2_ClrVal(); /* CLOCK LOW PULSE */&lt;BR /&gt; Delay();&lt;BR /&gt; Write((byte)(addr + READ));&lt;BR /&gt; Acknowledge = GetAck();&lt;BR /&gt; --Trial;&lt;BR /&gt; } &lt;BR /&gt; while((Trial != 0U) &amp;amp;&amp;amp; Acknowledge);&lt;BR /&gt; &lt;BR /&gt; if(Acknowledge) &lt;BR /&gt; {&lt;BR /&gt; IIC_9288_OnNACK();&lt;BR /&gt; Inhr2_SetDir((bool)OUTPUT);&lt;BR /&gt; Inhr2_ClrVal(); /* CLOCK LOW PULSE */&lt;BR /&gt; InternalStop();&lt;BR /&gt; return ERR_BUSY;&lt;BR /&gt; }&lt;BR /&gt; else &lt;BR /&gt; {&lt;BR /&gt; Inhr2_SetDir((bool)OUTPUT);&lt;BR /&gt; Inhr2_ClrVal(); /* CLOCK LOW PULSE */&lt;BR /&gt; Delay();&lt;BR /&gt; }&lt;BR /&gt; &lt;BR /&gt; for (I = 0U; I &amp;lt; Siz; I++)&lt;BR /&gt; {&lt;BR /&gt; *((byte *) Ptr + I) = Read();&lt;BR /&gt; IIC_9288_OnRxChar();&lt;BR /&gt; if (I == (Siz - 1U)) &lt;BR /&gt; {&lt;BR /&gt; SetAck((bool)NOACK);&lt;BR /&gt; }&lt;BR /&gt; else&lt;BR /&gt; {&lt;BR /&gt; SetAck((bool)ACK);&lt;BR /&gt; }&lt;BR /&gt; ++(*Rcv);&lt;BR /&gt; }&lt;BR /&gt; return ERR_OK;&lt;BR /&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Feb 2018 02:38:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-Read-iic-for-the-S12G64/m-p/775806#M15457</guid>
      <dc:creator>yanlaidong</dc:creator>
      <dc:date>2018-02-01T02:38:37Z</dc:date>
    </item>
    <item>
      <title>Re: How to Read iic for the S12G64?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-Read-iic-for-the-S12G64/m-p/775807#M15458</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;When you monitor the communication on the SDA, SCL pins, do you get correct response from MAX9288?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Feb 2018 15:44:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-Read-iic-for-the-S12G64/m-p/775807#M15458</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-02-01T15:44:19Z</dc:date>
    </item>
  </channel>
</rss>