<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックOur flash cotent is not sufficient, Can the Dflash used as code flash?</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Our-flash-cotent-is-not-sufficient-Can-the-Dflash-used-as-code/m-p/754970#M15158</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Our project has some picture, and our customer want us add more, but our flash rom was not sufficient, so I wander is it possible to put some picture or function in the data flash.But when I test putted a const data in the dflash and compile,&amp;nbsp; the data was not in the target file, when I putted the data in the p-flash , it was correct! Is it the compilled restrict this or dflash can't excute fucntion?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 Dec 2017 06:54:06 GMT</pubDate>
    <dc:creator>hongjianzhang</dc:creator>
    <dc:date>2017-12-01T06:54:06Z</dc:date>
    <item>
      <title>Our flash cotent is not sufficient, Can the Dflash used as code flash?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Our-flash-cotent-is-not-sufficient-Can-the-Dflash-used-as-code/m-p/754970#M15158</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Our project has some picture, and our customer want us add more, but our flash rom was not sufficient, so I wander is it possible to put some picture or function in the data flash.But when I test putted a const data in the dflash and compile,&amp;nbsp; the data was not in the target file, when I putted the data in the p-flash , it was correct! Is it the compilled restrict this or dflash can't excute fucntion?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Dec 2017 06:54:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Our-flash-cotent-is-not-sufficient-Can-the-Dflash-used-as-code/m-p/754970#M15158</guid>
      <dc:creator>hongjianzhang</dc:creator>
      <dc:date>2017-12-01T06:54:06Z</dc:date>
    </item>
    <item>
      <title>Re: Our flash cotent is not sufficient, Can the Dflash used as code flash?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Our-flash-cotent-is-not-sufficient-Can-the-Dflash-used-as-code/m-p/754971#M15159</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;you have not mentioned the MCU you use.&lt;/P&gt;&lt;P&gt;However, I think&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/450421"&gt;https://community.nxp.com/thread/450421&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;answers your issue.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ladislav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Dec 2017 12:51:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Our-flash-cotent-is-not-sufficient-Can-the-Dflash-used-as-code/m-p/754971#M15159</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2017-12-05T12:51:01Z</dc:date>
    </item>
  </channel>
</rss>