<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックSCI0 initialization on mc9s12g</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/SCI0-initialization-on-mc9s12g/m-p/749340#M15106</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everybody,&lt;/P&gt;&lt;P&gt;I need to implement SCI0 on MC9S12G240 and MC9S12G128. I create files header and C following&amp;nbsp;AN2485 (not the same file, but more function are the same). To test my project I used TWR-S12G240 demoboard. I connect some test point on PS0 and PS1, but when I launch my program I don't see anything. I debug my program with my Codewarrior IDE and I see that interrupt is working (I put a breakpoint in the interrupt function and I see that the program enter in it until it ends the buffer transmission).&lt;/P&gt;&lt;P&gt;My question is: how can I set the PS0 and PS1 bit to have 2nd function (TxD and RxD).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;many thanks and BR,&lt;/P&gt;&lt;P&gt;Andrea Cavazzoni&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Dec 2017 10:54:14 GMT</pubDate>
    <dc:creator>andreacavazzoni</dc:creator>
    <dc:date>2017-12-27T10:54:14Z</dc:date>
    <item>
      <title>SCI0 initialization on mc9s12g</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/SCI0-initialization-on-mc9s12g/m-p/749340#M15106</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everybody,&lt;/P&gt;&lt;P&gt;I need to implement SCI0 on MC9S12G240 and MC9S12G128. I create files header and C following&amp;nbsp;AN2485 (not the same file, but more function are the same). To test my project I used TWR-S12G240 demoboard. I connect some test point on PS0 and PS1, but when I launch my program I don't see anything. I debug my program with my Codewarrior IDE and I see that interrupt is working (I put a breakpoint in the interrupt function and I see that the program enter in it until it ends the buffer transmission).&lt;/P&gt;&lt;P&gt;My question is: how can I set the PS0 and PS1 bit to have 2nd function (TxD and RxD).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;many thanks and BR,&lt;/P&gt;&lt;P&gt;Andrea Cavazzoni&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Dec 2017 10:54:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/SCI0-initialization-on-mc9s12g/m-p/749340#M15106</guid>
      <dc:creator>andreacavazzoni</dc:creator>
      <dc:date>2017-12-27T10:54:14Z</dc:date>
    </item>
    <item>
      <title>Re: SCI0 initialization on mc9s12g</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/SCI0-initialization-on-mc9s12g/m-p/749341#M15107</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everybody, I solved my trouble.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Dec 2017 08:54:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/SCI0-initialization-on-mc9s12g/m-p/749341#M15107</guid>
      <dc:creator>andreacavazzoni</dc:creator>
      <dc:date>2017-12-28T08:54:28Z</dc:date>
    </item>
  </channel>
</rss>