<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S12ZVL maximum supply voltage in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL-maximum-supply-voltage/m-p/747193#M15085</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;I have to modify my previous answer. Based on the last information I have received, the footnote:&lt;BR /&gt;“Operation in the range 20V&amp;lt;VSUP&amp;lt;26.5V is limited to 1 hour over lifetime of the device. In this range the device continues to function but electrical parameters are degraded",&lt;BR /&gt;will not be removed as I was informed two weeks ago but modified to:&lt;BR /&gt;“Operation up to VSUP=28.5V is limited to 1 hour over lifetime of the device. In this range the device continues to function but electrical parameters are degraded.”&lt;/P&gt;&lt;P&gt;But this doesn’t mean that the device can be used at this voltage continuously. &lt;BR /&gt;MagniV devices target 12V application and can be used continuously at voltage up to 18V.&lt;BR /&gt;There is &lt;A href="https://www.nxp.com/docs/en/application-note/AN5082.pdf"&gt;AN5082 MagniV in 24V Applications&lt;/A&gt;&amp;nbsp;you can refer to.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Jun 2018 09:54:52 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2018-06-06T09:54:52Z</dc:date>
    <item>
      <title>S12ZVL maximum supply voltage</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL-maximum-supply-voltage/m-p/747192#M15084</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the maximum supply voltage to S12ZVL?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see that it is documented to be a 12V/18V nominal supply voltage. There is also a note in the reference manual that&amp;nbsp; "&lt;SPAN class=""&gt;Operation in the range 20V&amp;lt;VSUP&amp;lt;26.5V is limited to 1 hour over lifetime of the&lt;BR /&gt;device. In this range the device continues to function but electrical parameters are degraded&lt;/SPAN&gt;&amp;nbsp;".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an existing system with a 19.8V power supply. Can I use this to power the S12ZVL?&lt;/P&gt;&lt;P&gt;More particularly:&lt;/P&gt;&lt;P&gt;a) What happens if say I operate from a 23V power supply. Can I do this permanently if&amp;nbsp; I can accept "&lt;SPAN class=""&gt;electrical parameters are degraded&lt;/SPAN&gt;". (I am NOT using the S12ZVL for any analogue function)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Jun 2018 00:00:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL-maximum-supply-voltage/m-p/747192#M15084</guid>
      <dc:creator>huang_hw</dc:creator>
      <dc:date>2018-06-04T00:00:21Z</dc:date>
    </item>
    <item>
      <title>Re: S12ZVL maximum supply voltage</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL-maximum-supply-voltage/m-p/747193#M15085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;I have to modify my previous answer. Based on the last information I have received, the footnote:&lt;BR /&gt;“Operation in the range 20V&amp;lt;VSUP&amp;lt;26.5V is limited to 1 hour over lifetime of the device. In this range the device continues to function but electrical parameters are degraded",&lt;BR /&gt;will not be removed as I was informed two weeks ago but modified to:&lt;BR /&gt;“Operation up to VSUP=28.5V is limited to 1 hour over lifetime of the device. In this range the device continues to function but electrical parameters are degraded.”&lt;/P&gt;&lt;P&gt;But this doesn’t mean that the device can be used at this voltage continuously. &lt;BR /&gt;MagniV devices target 12V application and can be used continuously at voltage up to 18V.&lt;BR /&gt;There is &lt;A href="https://www.nxp.com/docs/en/application-note/AN5082.pdf"&gt;AN5082 MagniV in 24V Applications&lt;/A&gt;&amp;nbsp;you can refer to.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jun 2018 09:54:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVL-maximum-supply-voltage/m-p/747193#M15085</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-06-06T09:54:52Z</dc:date>
    </item>
  </channel>
</rss>