<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Issue about the MC9S12XEP100 CLOCK Circuit in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Issue-about-the-MC9S12XEP100-CLOCK-Circuit/m-p/738583#M14972</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; My issue is about the MCU clock circuit,,below is the description of the issue:&lt;/P&gt;&lt;P&gt;===========================Issue Description=============================&lt;/P&gt;&lt;P&gt;My product 's MCU is MC9S12XEP100,MCU circuit and the product can work nomaly,but some products(&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;About 2% of the total, so far&lt;/SPAN&gt;&lt;/SPAN&gt;) &lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;occur the phenomenon of abnormal work after about two years used,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;The specific phenomenon is：the MCU's PLL can not stable,or occur crashes after run some time.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;The MCU's clock circuit design as below:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;IMG class="" data-bd-imgshare-binded="1" src="http://www.nxpic.org/module/forum/data/attachment/forum/201711/22/165315ta2pohu5ru53ut3u.png" width="495" /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;the picture above is the Crystal circuit,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;and the XCLKS pin not connect the pull-down，it is suspended;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;the MODA and MODB connect the pull-down;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;===========================Troubleshoot=============================&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;In troubleshooting the process described above, we found that there are two obvious deviations in the design:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;1.The Crystal&amp;nbsp; output the 5V&amp;nbsp; square wave,Obviously exceed EXTAL maximum 2.16V input requirement;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;2.XCLKS pin not pulled down;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;Then make the following changes to the clock circuit of the MCU on the circuit board of the failed product (the MCU's PLL can not be locked occasionally):&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/36014i343384AB1C9E69BB/image-size/large?v=v2&amp;amp;px=999" title="4.png" alt="4.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;At the same time the XCLKS foot drop pull, MODA, MODB and before, pick up the pull-down;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;After the above circuit is modified, the MCU still can not lock the PLL; when the crystal oscillator outputs 5V square wave, the PLL can lock occasionally. After the above modification, basically no PLL lock occurs.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;=============================Issue advisory===================================&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;The above is the specific phenomenon of the problem, then my question is:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;1. I suspect the crystal oscillator directly outputs 5V square wave to the EXTAL pin, causing the internal clock module of the MCU to malfunction. As a result, the PLL can not be locked, but I just wonder how to determine that the 5V square wave has caused the MCU internal Clock module failure?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;2. Why do the above MCUs have a normal working time of nearly 2 years under the condition that there are 2 parts that do not meet the requirements?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks!&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Nov 2017 03:26:58 GMT</pubDate>
    <dc:creator>xiaochenqiang</dc:creator>
    <dc:date>2017-11-27T03:26:58Z</dc:date>
    <item>
      <title>Issue about the MC9S12XEP100 CLOCK Circuit</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Issue-about-the-MC9S12XEP100-CLOCK-Circuit/m-p/738583#M14972</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; My issue is about the MCU clock circuit,,below is the description of the issue:&lt;/P&gt;&lt;P&gt;===========================Issue Description=============================&lt;/P&gt;&lt;P&gt;My product 's MCU is MC9S12XEP100,MCU circuit and the product can work nomaly,but some products(&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;About 2% of the total, so far&lt;/SPAN&gt;&lt;/SPAN&gt;) &lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;occur the phenomenon of abnormal work after about two years used,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;The specific phenomenon is：the MCU's PLL can not stable,or occur crashes after run some time.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;The MCU's clock circuit design as below:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;IMG class="" data-bd-imgshare-binded="1" src="http://www.nxpic.org/module/forum/data/attachment/forum/201711/22/165315ta2pohu5ru53ut3u.png" width="495" /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;the picture above is the Crystal circuit,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;and the XCLKS pin not connect the pull-down，it is suspended;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;the MODA and MODB connect the pull-down;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;===========================Troubleshoot=============================&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;In troubleshooting the process described above, we found that there are two obvious deviations in the design:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;1.The Crystal&amp;nbsp; output the 5V&amp;nbsp; square wave,Obviously exceed EXTAL maximum 2.16V input requirement;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;2.XCLKS pin not pulled down;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;Then make the following changes to the clock circuit of the MCU on the circuit board of the failed product (the MCU's PLL can not be locked occasionally):&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/36014i343384AB1C9E69BB/image-size/large?v=v2&amp;amp;px=999" title="4.png" alt="4.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;At the same time the XCLKS foot drop pull, MODA, MODB and before, pick up the pull-down;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;After the above circuit is modified, the MCU still can not lock the PLL; when the crystal oscillator outputs 5V square wave, the PLL can lock occasionally. After the above modification, basically no PLL lock occurs.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;=============================Issue advisory===================================&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;The above is the specific phenomenon of the problem, then my question is:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;1. I suspect the crystal oscillator directly outputs 5V square wave to the EXTAL pin, causing the internal clock module of the MCU to malfunction. As a result, the PLL can not be locked, but I just wonder how to determine that the 5V square wave has caused the MCU internal Clock module failure?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;2. Why do the above MCUs have a normal working time of nearly 2 years under the condition that there are 2 parts that do not meet the requirements?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks!&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Nov 2017 03:26:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Issue-about-the-MC9S12XEP100-CLOCK-Circuit/m-p/738583#M14972</guid>
      <dc:creator>xiaochenqiang</dc:creator>
      <dc:date>2017-11-27T03:26:58Z</dc:date>
    </item>
    <item>
      <title>Re: Issue about the MC9S12XEP100 CLOCK Circuit</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Issue-about-the-MC9S12XEP100-CLOCK-Circuit/m-p/738584#M14973</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using oscillator and any of MCU’s pins out of nominal values is really ticking time bomb. Maximum oscillator voltage can be Vddpll+0.3V. Voltage above this will cause higher current flow through internal circuits and because of electromigration it can cause oscillator circuitry damage anytime. Beyond absolute maximum ratings device might be damaged.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We solved similar issue where the customer had been using the device with 5V voltage level on Extal pin without problems for 2 years and then the device was damaged.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is electromigration which means the conductive material is carried from place to place which is caused by overcurrent and two things can happen:&lt;/P&gt;&lt;P&gt;1) Wire will be interrupted and MCU loses clocks. The thinner wire the higher local temperature =&amp;gt; local overheating can cause degradation of ambient integrated circuits.&lt;/P&gt;&lt;P&gt;2) Accumulated conductive material on another place will cause short cut with another line =&amp;gt; anything can happen.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Maybe the failure is detectable but nobody tested it because such conditions are out of specifications required by data sheet. I am sorry but nothing is printed or available or qualified for the public on this topic.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have also contacted design team to get more info and I received the same answer as I have provided to you; citation:&lt;/P&gt;&lt;P&gt;”FSL&amp;nbsp;cannot give any guarantee for operation when 5V is applied to the EXTAL pin, since this is far out of the specification”&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can find in the attachment EVB design as well as you can find some notes to design in:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-93813"&gt;https://community.nxp.com/docs/DOC-93813&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards, Ladislav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Nov 2017 17:46:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Issue-about-the-MC9S12XEP100-CLOCK-Circuit/m-p/738584#M14973</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2017-11-27T17:46:26Z</dc:date>
    </item>
    <item>
      <title>Re: Issue about the MC9S12XEP100 CLOCK Circuit</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Issue-about-the-MC9S12XEP100-CLOCK-Circuit/m-p/738585#M14974</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi lama:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks,I want to know how to verify the MCU's oscillator circuitry has damaged,if the design team tell you more info about it ,please tell me in time,because this is very urgent.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; thans again!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Nov 2017 01:34:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Issue-about-the-MC9S12XEP100-CLOCK-Circuit/m-p/738585#M14974</guid>
      <dc:creator>xiaochenqiang</dc:creator>
      <dc:date>2017-11-28T01:34:05Z</dc:date>
    </item>
    <item>
      <title>Re: Issue about the MC9S12XEP100 CLOCK Circuit</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Issue-about-the-MC9S12XEP100-CLOCK-Circuit/m-p/738586#M14975</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,lama:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Have you get the reply of the design team? M&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;y problem is very urgent&lt;/SPAN&gt;&lt;/SPAN&gt;，Please&amp;nbsp; &lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;contact the design team again,thank you very much!!&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Dec 2017 01:13:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Issue-about-the-MC9S12XEP100-CLOCK-Circuit/m-p/738586#M14975</guid>
      <dc:creator>xiaochenqiang</dc:creator>
      <dc:date>2017-12-05T01:13:07Z</dc:date>
    </item>
    <item>
      <title>Re: Issue about the MC9S12XEP100 CLOCK Circuit</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Issue-about-the-MC9S12XEP100-CLOCK-Circuit/m-p/738587#M14976</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;it looks like you incorrectly understood my message:&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;I have also contacted design team to get more info and I received the same answer as I have provided to you; citation:&lt;/P&gt;&lt;P&gt;”FSL&amp;nbsp;cannot give any guarantee for operation when 5V is applied to the EXTAL pin, since this is far out of the specification”&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Their answer was in the brackets. I have no more info from them.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ladislav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Dec 2017 12:52:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Issue-about-the-MC9S12XEP100-CLOCK-Circuit/m-p/738587#M14976</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2017-12-05T12:52:58Z</dc:date>
    </item>
    <item>
      <title>Re: Issue about the MC9S12XEP100 CLOCK Circuit</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Issue-about-the-MC9S12XEP100-CLOCK-Circuit/m-p/738588#M14977</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,lama:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I understand the wrong used,I want to know how to v&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;erify the problem,Can the design team provide any way to v&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;erify the MCU'S &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN&gt;internal clock module have Damaged？&lt;/SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Thank you!&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Dec 2017 05:08:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Issue-about-the-MC9S12XEP100-CLOCK-Circuit/m-p/738588#M14977</guid>
      <dc:creator>xiaochenqiang</dc:creator>
      <dc:date>2017-12-06T05:08:37Z</dc:date>
    </item>
    <item>
      <title>Re: Issue about the MC9S12XEP100 CLOCK Circuit</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Issue-about-the-MC9S12XEP100-CLOCK-Circuit/m-p/738589#M14978</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, the easiest test is to start the MCU in the special single chip mode (pins MODC=MODB=MODA=0) and test the BUSCLK at the pin. In this mode NECLK bit is 0 which provides BUSCLK at pin PE4 which should be OSCCLK/2.&amp;nbsp; If there is frequency between 500kHz~2MHz then the MCU is in the self clock mode and you have wrong input clock or oscillator circuitry is damaged. If there is nothing at the pin then MCU is damaged. &lt;/P&gt;&lt;P&gt;(For more info about self clock mode please read the data sheet)&lt;/P&gt;&lt;P&gt;Best regrads,&lt;/P&gt;&lt;P&gt;Ladislav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Dec 2017 12:31:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Issue-about-the-MC9S12XEP100-CLOCK-Circuit/m-p/738589#M14978</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2017-12-07T12:31:53Z</dc:date>
    </item>
    <item>
      <title>Re: Issue about the MC9S12XEP100 CLOCK Circuit</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Issue-about-the-MC9S12XEP100-CLOCK-Circuit/m-p/738590#M14979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi，&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;based on&amp;nbsp; first picture circuit&lt;/SPAN&gt;&lt;/SPAN&gt;,I connect the MODC to the GDN,and then test the pin PE4,it is the OSCCLK/2,so the oscillator circuitry is not damaged?but some times, the MCU can not work normaly,because the PLL can not stable.why?&lt;/P&gt;&lt;P&gt;Below is the test scope:&lt;/P&gt;&lt;P&gt;the input clock is 16M,and the test scope is 8M,&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2567i8A6DADC952254E3F/image-size/large?v=v2&amp;amp;px=999" title="1.jpg" alt="1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Dec 2017 02:18:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Issue-about-the-MC9S12XEP100-CLOCK-Circuit/m-p/738590#M14979</guid>
      <dc:creator>xiaochenqiang</dc:creator>
      <dc:date>2017-12-08T02:18:19Z</dc:date>
    </item>
    <item>
      <title>Re: Issue about the MC9S12XEP100 CLOCK Circuit</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Issue-about-the-MC9S12XEP100-CLOCK-Circuit/m-p/738591#M14980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi lama:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Maybe the MCU's internal CLOCK circuit realy damaged;following is the scope of the test on the PE4 (the yellow scope），&lt;/P&gt;&lt;P&gt;the test &lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;phenomenon&lt;/SPAN&gt;&lt;/SPAN&gt; is: After the power on,the MCU can work normaly for some time,when it can work normaly,the yellow scope is the 5V High level,&lt;/P&gt;&lt;P&gt;and after some time(the time is random),the MCU can not work normaly,the scope changed from 5V high level to 5V square，and the square's frequency&amp;nbsp; not same every time;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Can you explain why it occur this &lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;phenomenon&lt;/SPAN&gt;&lt;/SPAN&gt; ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; when the PE4 become the square，it enter the internal clock mode?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thank you!&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30248i4F26FBF7985B3925/image-size/large?v=v2&amp;amp;px=999" title="1.jpg" alt="1.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30302i071BAFC1941F2607/image-size/large?v=v2&amp;amp;px=999" title="2.jpg" alt="2.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30303iC84CC34F822CD1D9/image-size/large?v=v2&amp;amp;px=999" title="3.jpg" alt="3.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30333i91D7CB104B69381C/image-size/large?v=v2&amp;amp;px=999" title="4.jpg" alt="4.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30340iEA1DD78AC01F78B1/image-size/large?v=v2&amp;amp;px=999" title="5.jpg" alt="5.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30394i6C6F0FC8D93D64FD/image-size/large?v=v2&amp;amp;px=999" title="6.jpg" alt="6.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Dec 2017 08:46:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Issue-about-the-MC9S12XEP100-CLOCK-Circuit/m-p/738591#M14980</guid>
      <dc:creator>xiaochenqiang</dc:creator>
      <dc:date>2017-12-20T08:46:18Z</dc:date>
    </item>
  </channel>
</rss>