<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: Flash write</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flash-write/m-p/734949#M14926</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;By writing FSTAT_CCIF = 1, you launch the flash command. &lt;BR /&gt;Please make sure you don’t launch the command from the same flash block.&lt;BR /&gt;You may refer to&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-333063"&gt;S12Z Flash example code&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the example, you can place the code either into RAM or execute the code&amp;nbsp;in an array of instruction in machine code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 16 Apr 2018 15:49:02 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2018-04-16T15:49:02Z</dc:date>
    <item>
      <title>Flash write</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flash-write/m-p/734948#M14925</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I wanna write some data in P-Flash with MC9S12ZVCA192. When I debug the program with step by step, the data can write P-Flash. But When I run the program in debug, it was paused in the FSTAT_CCIF = 1. When I check FSTAT register, I find it data was 00001000b.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Apr 2018 07:10:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flash-write/m-p/734948#M14925</guid>
      <dc:creator>wangzhongyuan</dc:creator>
      <dc:date>2018-04-16T07:10:26Z</dc:date>
    </item>
    <item>
      <title>Re: Flash write</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flash-write/m-p/734949#M14926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;By writing FSTAT_CCIF = 1, you launch the flash command. &lt;BR /&gt;Please make sure you don’t launch the command from the same flash block.&lt;BR /&gt;You may refer to&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-333063"&gt;S12Z Flash example code&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the example, you can place the code either into RAM or execute the code&amp;nbsp;in an array of instruction in machine code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Apr 2018 15:49:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flash-write/m-p/734949#M14926</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-04-16T15:49:02Z</dc:date>
    </item>
  </channel>
</rss>