<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic About sleep current on 9S12ZVL32F0MLC in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/About-sleep-current-on-9S12ZVL32F0MLC/m-p/733359#M14914</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The circuit diagrams in my project in the attachment as picture 1, if set pin9 and pin12 as pull-up output, the sleep current of mcu is 20uA higher than which is set as pull-up input. Could you help to explain it. Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;R10 is equivalent to the internal pull-up resistance of&amp;nbsp;MCU,other resistors are external components&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 May 2018 03:01:58 GMT</pubDate>
    <dc:creator>binhuang</dc:creator>
    <dc:date>2018-05-30T03:01:58Z</dc:date>
    <item>
      <title>About sleep current on 9S12ZVL32F0MLC</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/About-sleep-current-on-9S12ZVL32F0MLC/m-p/733359#M14914</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The circuit diagrams in my project in the attachment as picture 1, if set pin9 and pin12 as pull-up output, the sleep current of mcu is 20uA higher than which is set as pull-up input. Could you help to explain it. Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;R10 is equivalent to the internal pull-up resistance of&amp;nbsp;MCU,other resistors are external components&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 May 2018 03:01:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/About-sleep-current-on-9S12ZVL32F0MLC/m-p/733359#M14914</guid>
      <dc:creator>binhuang</dc:creator>
      <dc:date>2018-05-30T03:01:58Z</dc:date>
    </item>
  </channel>
</rss>