<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S12G64 PWM output error in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12G64-PWM-output-error/m-p/732105#M14907</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Problem Description: Normally, the firmware output a PWM of constant 80% duty cycle and 2.5KHz frequency by PWM1 port. After our device has run several hours, the PWM output change to constant 1% duty cycle and 2.5KHz. The 1% duty must not be set by firmware, it is a abnormal value. I had try to turn off the device and power-on again, and reset the MCU by /RESET pin, but the error state is still held. Then i try to burn the firmware into flash by BDM, the error is removed and the duty of PWM output is normal. Additional, i had check the firmware image by reading from the fault device by BDM, the image is same with the normal one. &lt;/P&gt;&lt;P&gt;Please help&amp;nbsp;to analysis the error. Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Dec 2017 02:49:26 GMT</pubDate>
    <dc:creator>xiaoqingli</dc:creator>
    <dc:date>2017-12-19T02:49:26Z</dc:date>
    <item>
      <title>S12G64 PWM output error</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12G64-PWM-output-error/m-p/732105#M14907</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Problem Description: Normally, the firmware output a PWM of constant 80% duty cycle and 2.5KHz frequency by PWM1 port. After our device has run several hours, the PWM output change to constant 1% duty cycle and 2.5KHz. The 1% duty must not be set by firmware, it is a abnormal value. I had try to turn off the device and power-on again, and reset the MCU by /RESET pin, but the error state is still held. Then i try to burn the firmware into flash by BDM, the error is removed and the duty of PWM output is normal. Additional, i had check the firmware image by reading from the fault device by BDM, the image is same with the normal one. &lt;/P&gt;&lt;P&gt;Please help&amp;nbsp;to analysis the error. Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Dec 2017 02:49:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12G64-PWM-output-error/m-p/732105#M14907</guid>
      <dc:creator>xiaoqingli</dc:creator>
      <dc:date>2017-12-19T02:49:26Z</dc:date>
    </item>
    <item>
      <title>Re: S12G64 PWM output error</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12G64-PWM-output-error/m-p/732106#M14908</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Can you reproduce the fault? Have you tried another chip?&lt;/P&gt;&lt;P&gt;Do you initialize the PWMDTYx register with a constant or a variable/pointer?&lt;/P&gt;&lt;P&gt;Does the rest of the MCU work correctly during the PWM failure?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Dec 2017 16:03:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12G64-PWM-output-error/m-p/732106#M14908</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-12-20T16:03:12Z</dc:date>
    </item>
    <item>
      <title>Re: S12G64 PWM output error</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12G64-PWM-output-error/m-p/732107#M14909</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;After&amp;nbsp;the fault is removed by re-burn the flash, these deives has been running for about twenty-four hours, currently they seem normal. The rest of MCU should be working correctly, such as CAN communication, we can read state and control the deivce ON/OFF by CAN, but changing duty by CAN is invalid, in other words, only the PWM duty part is abnormal.&lt;/P&gt;&lt;P&gt;While running without external CAN command, the PWMDTY01 register is set with a two bytes constant.&lt;/P&gt;&lt;P&gt;In the previous test, ten of evleven devices has the failure, then we thought it is a common phenomenon, so we don't try another chip.&lt;/P&gt;&lt;P&gt;Daniel, thanks for your support.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Dec 2017 00:32:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12G64-PWM-output-error/m-p/732107#M14909</guid>
      <dc:creator>xiaoqingli</dc:creator>
      <dc:date>2017-12-21T00:32:28Z</dc:date>
    </item>
  </channel>
</rss>