<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Default level of GPIO  in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Default-level-of-GPIO/m-p/718265#M14795</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the default level of GPIO after S12XET256 &amp;nbsp;power up and befor control？&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Mar 2018 03:26:40 GMT</pubDate>
    <dc:creator>528887301</dc:creator>
    <dc:date>2018-03-01T03:26:40Z</dc:date>
    <item>
      <title>Default level of GPIO</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Default-level-of-GPIO/m-p/718265#M14795</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the default level of GPIO after S12XET256 &amp;nbsp;power up and befor control？&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Mar 2018 03:26:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Default-level-of-GPIO/m-p/718265#M14795</guid>
      <dc:creator>528887301</dc:creator>
      <dc:date>2018-03-01T03:26:40Z</dc:date>
    </item>
    <item>
      <title>Re: Default level of GPIO</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Default-level-of-GPIO/m-p/718266#M14796</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the RM you can see specification for each available port. Some of them has GPIO function after reset. In the DDRx register for&amp;nbsp;&lt;SPAN&gt;associated port&amp;nbsp;&lt;/SPAN&gt;you can see default state for associated pin. For example, Port P is configured as input (see DDRP) and in the PERP register you can see default state of pull device. Pull device is disabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Mar 2018 13:47:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Default-level-of-GPIO/m-p/718266#M14796</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2018-03-05T13:47:17Z</dc:date>
    </item>
  </channel>
</rss>