<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: AN5327(3-phase Sensorless Single-Shunt Current) question in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/AN5327-3-phase-Sensorless-Single-Shunt-Current-question/m-p/712394#M14732</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear&amp;nbsp;BJ Hwang,&lt;/P&gt;&lt;P&gt;As far as I know, there is no example available combining LIN communication and motor control application for S12ZVML.&lt;/P&gt;&lt;P&gt;But you can combine two application notes AN5327 and AN5122 available at&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/s12zvm" title="https://www.nxp.com/s12zvm"&gt;S12ZVM Mixed-Signal MCUs|MagniV|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Since the AN5327 is controlled by FreeMASTER&amp;nbsp;- MCAT interface, the only change would be necessary only if the SCI hardware pins overlap the LIN communication pins. Then you would have a possibility to debug the communication using FreeMASTER as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Matej&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Sep 2017 06:59:17 GMT</pubDate>
    <dc:creator>pachamatej</dc:creator>
    <dc:date>2017-09-26T06:59:17Z</dc:date>
    <item>
      <title>AN5327(3-phase Sensorless Single-Shunt Current) question</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/AN5327-3-phase-Sensorless-Single-Shunt-Current-question/m-p/712393#M14731</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Sir or Madam,&lt;/P&gt;&lt;P&gt;I have a question related to this AN5327SW.&lt;/P&gt;&lt;P&gt;Currently, this SW runs the motor by using MCAT tool.&lt;/P&gt;&lt;P&gt;Is there some advice or other example that runs with LIN communication?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Sep 2017 02:26:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/AN5327-3-phase-Sensorless-Single-Shunt-Current-question/m-p/712393#M14731</guid>
      <dc:creator>bjhwang</dc:creator>
      <dc:date>2017-09-25T02:26:30Z</dc:date>
    </item>
    <item>
      <title>Re: AN5327(3-phase Sensorless Single-Shunt Current) question</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/AN5327-3-phase-Sensorless-Single-Shunt-Current-question/m-p/712394#M14732</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear&amp;nbsp;BJ Hwang,&lt;/P&gt;&lt;P&gt;As far as I know, there is no example available combining LIN communication and motor control application for S12ZVML.&lt;/P&gt;&lt;P&gt;But you can combine two application notes AN5327 and AN5122 available at&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/s12zvm" title="https://www.nxp.com/s12zvm"&gt;S12ZVM Mixed-Signal MCUs|MagniV|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Since the AN5327 is controlled by FreeMASTER&amp;nbsp;- MCAT interface, the only change would be necessary only if the SCI hardware pins overlap the LIN communication pins. Then you would have a possibility to debug the communication using FreeMASTER as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Matej&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Sep 2017 06:59:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/AN5327-3-phase-Sensorless-Single-Shunt-Current-question/m-p/712394#M14732</guid>
      <dc:creator>pachamatej</dc:creator>
      <dc:date>2017-09-26T06:59:17Z</dc:date>
    </item>
    <item>
      <title>Re: AN5327(3-phase Sensorless Single-Shunt Current) question</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/AN5327-3-phase-Sensorless-Single-Shunt-Current-question/m-p/712395#M14733</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Sir,&lt;/P&gt;&lt;P&gt;Thank you for the reply. From your advice I tried to combine the application note AN5327 / AN5122.&lt;/P&gt;&lt;P&gt;Not like application notes, I set the MCU slave S12ZVML128 and made cfg file. After that I put all the LIN Driver from the AN5122 to AN5327 and made access path to it also. Lastly, I include "Lin.h" and build the project. The compile progress was ok, but when I debug this application notes, &lt;STRONG&gt;this&amp;nbsp;failed to resume target process. downloading binary to target...&amp;nbsp;&lt;/STRONG&gt;messages comes out.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you tell me this?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Oct 2017 02:35:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/AN5327-3-phase-Sensorless-Single-Shunt-Current-question/m-p/712395#M14733</guid>
      <dc:creator>bjhwang</dc:creator>
      <dc:date>2017-10-18T02:35:01Z</dc:date>
    </item>
  </channel>
</rss>