<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: About MC9S12Dx512's MMC-Memory-map file.</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/About-MC9S12Dx512-s-MMC-Memory-map-file/m-p/710375#M14700</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, you can us it directly. However, it is necessary to read the entire AN3275.pdf carefully.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best reards,&lt;/P&gt;&lt;P&gt;Ladislav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Oct 2017 21:08:56 GMT</pubDate>
    <dc:creator>lama</dc:creator>
    <dc:date>2017-10-19T21:08:56Z</dc:date>
    <item>
      <title>About MC9S12Dx512's MMC-Memory-map file.</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/About-MC9S12Dx512-s-MMC-Memory-map-file/m-p/710372#M14697</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI&lt;/P&gt;&lt;P&gt;I am now doing a bootloader based on the MC9S12DP512, but now I have &amp;nbsp;some problems. Flash on the use of the time to use the address, I should use the global address or PPAGE configuration selection erase it. Can you give me a memory map? There is no single-chip internal address register? I can not find the relevant introduction in the chip manual.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Oct 2017 07:32:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/About-MC9S12Dx512-s-MMC-Memory-map-file/m-p/710372#M14697</guid>
      <dc:creator>yongpanan</dc:creator>
      <dc:date>2017-10-19T07:32:26Z</dc:date>
    </item>
    <item>
      <title>Re: About MC9S12Dx512's MMC-Memory-map file.</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/About-MC9S12Dx512-s-MMC-Memory-map-file/m-p/710373#M14698</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;there is no globla memory approach. In order to be access any part of the flash you can use 16bit address only for spaces 4000~7FFF and C000~FFFF which are also addressable via PPAGE access via pages 3E and 3F together with window 8000~BFFF.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Moreover, the memory map can be affected by modification registers INITRG, INITRM and INITEE.&lt;/P&gt;&lt;P&gt;The memory map can be found in the attachment.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Moreover, I have attached a SW which can help you to create your own bootloader.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ladislav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Oct 2017 10:04:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/About-MC9S12Dx512-s-MMC-Memory-map-file/m-p/710373#M14698</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2017-10-19T10:04:55Z</dc:date>
    </item>
    <item>
      <title>Re: About MC9S12Dx512's MMC-Memory-map file.</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/About-MC9S12Dx512-s-MMC-Memory-map-file/m-p/710374#M14699</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks,&lt;BR /&gt;About the An3275SW ,Can I used for MC9S12DP512 directly?&lt;BR /&gt;If no,Which module did i should to modify?&lt;BR /&gt;I was the first to use this chip。And the AN3275SW is too diffcult for me to understanding.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Oct 2017 12:06:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/About-MC9S12Dx512-s-MMC-Memory-map-file/m-p/710374#M14699</guid>
      <dc:creator>yongpanan</dc:creator>
      <dc:date>2017-10-19T12:06:39Z</dc:date>
    </item>
    <item>
      <title>Re: About MC9S12Dx512's MMC-Memory-map file.</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/About-MC9S12Dx512-s-MMC-Memory-map-file/m-p/710375#M14700</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, you can us it directly. However, it is necessary to read the entire AN3275.pdf carefully.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best reards,&lt;/P&gt;&lt;P&gt;Ladislav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Oct 2017 21:08:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/About-MC9S12Dx512-s-MMC-Memory-map-file/m-p/710375#M14700</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2017-10-19T21:08:56Z</dc:date>
    </item>
    <item>
      <title>Re: About MC9S12Dx512's MMC-Memory-map file.</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/About-MC9S12Dx512-s-MMC-Memory-map-file/m-p/710376#M14701</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Got it.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Oct 2017 23:48:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/About-MC9S12Dx512-s-MMC-Memory-map-file/m-p/710376#M14701</guid>
      <dc:creator>yongpanan</dc:creator>
      <dc:date>2017-10-19T23:48:56Z</dc:date>
    </item>
  </channel>
</rss>