<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: AN5201(Integrating the LIN driver) question in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/AN5201-Integrating-the-LIN-driver-question/m-p/707748#M14670</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the feedback.&lt;/P&gt;&lt;P&gt;I have one more question to this AN5201SW.&lt;/P&gt;&lt;P&gt;You said that &lt;STRONG&gt;all the registers are written only once&lt;/STRONG&gt;, but I'm confuse about this.&lt;/P&gt;&lt;P&gt;The testing condition is same as I mentioned before(S12ZVMxEVB), and&amp;nbsp;If I perform reset(SW4) while the OSBDM is implemented the motor is not running.(the motor automatically runs at 1500RPM).&lt;/P&gt;&lt;P&gt;So the point is, if I change this registers to normal single chip mode, the board can performs reset and runs at 1500RPM again?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Best Regards&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Sep 2017 02:19:56 GMT</pubDate>
    <dc:creator>bjhwang</dc:creator>
    <dc:date>2017-09-25T02:19:56Z</dc:date>
    <item>
      <title>AN5201(Integrating the LIN driver) question</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/AN5201-Integrating-the-LIN-driver-question/m-p/707746#M14668</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Sir or Madam,&lt;/P&gt;&lt;P&gt;I'm using S12ZVMx128 EVB for testing LIN communication.&lt;/P&gt;&lt;P&gt;I use OSBDM port to debug the board and using AN5201SW for example.&lt;/P&gt;&lt;P&gt;The problem is the sw runs very well while OSBDM cable is inserted, but after reset(power switch off/on and the cable is removed), the motor is not running. It doesn't perform reset.&lt;/P&gt;&lt;P&gt;Could you give me some advice for this?&lt;/P&gt;&lt;P&gt;Thank you.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Sep 2017 07:39:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/AN5201-Integrating-the-LIN-driver-question/m-p/707746#M14668</guid>
      <dc:creator>bjhwang</dc:creator>
      <dc:date>2017-09-19T07:39:52Z</dc:date>
    </item>
    <item>
      <title>Re: AN5201(Integrating the LIN driver) question</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/AN5201-Integrating-the-LIN-driver-question/m-p/707747#M14669</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;With OSBDM, the MCU enters Special Single Chip Mode. See Chapter 1.9.1 of the reference manual.&lt;/P&gt;&lt;P&gt;Without the debugger, the MCU enters Normal Single Chip Mode.&lt;/P&gt;&lt;P&gt;Certain registers can be written only once in Normal Mode, for instance MODRR0/1,2, FOPT, CPMUCOP, …&lt;/P&gt;&lt;P&gt;Whereas in Special Mode, they can be written anytime.&lt;/P&gt;&lt;P&gt;So make sure all the registers are written only once.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Sep 2017 12:21:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/AN5201-Integrating-the-LIN-driver-question/m-p/707747#M14669</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-09-20T12:21:50Z</dc:date>
    </item>
    <item>
      <title>Re: AN5201(Integrating the LIN driver) question</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/AN5201-Integrating-the-LIN-driver-question/m-p/707748#M14670</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the feedback.&lt;/P&gt;&lt;P&gt;I have one more question to this AN5201SW.&lt;/P&gt;&lt;P&gt;You said that &lt;STRONG&gt;all the registers are written only once&lt;/STRONG&gt;, but I'm confuse about this.&lt;/P&gt;&lt;P&gt;The testing condition is same as I mentioned before(S12ZVMxEVB), and&amp;nbsp;If I perform reset(SW4) while the OSBDM is implemented the motor is not running.(the motor automatically runs at 1500RPM).&lt;/P&gt;&lt;P&gt;So the point is, if I change this registers to normal single chip mode, the board can performs reset and runs at 1500RPM again?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Best Regards&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Sep 2017 02:19:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/AN5201-Integrating-the-LIN-driver-question/m-p/707748#M14670</guid>
      <dc:creator>bjhwang</dc:creator>
      <dc:date>2017-09-25T02:19:56Z</dc:date>
    </item>
  </channel>
</rss>