<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックS12ZVM128 EVB LIN communication</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVM128-EVB-LIN-communication/m-p/706020#M14640</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Sir or Madam,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to ask you question about the S12ZVM128 EVB LIN communication.&lt;/P&gt;&lt;P&gt;Currently I have two &lt;SPAN&gt;S12ZVM128 EVB boards and&lt;/SPAN&gt;&amp;nbsp;found two application notes(AN5201, AN5122).&lt;/P&gt;&lt;P&gt;But one is using S12ZVR32EVB for master, a S12ZVM128EVB for slave(AN5201), and the other one uses a S12ZVM EVB as master, S12VR64 EVB as slave(AN5122).&lt;BR /&gt;So I tried to mixed these it up, but it doesn't work.&lt;/P&gt;&lt;P&gt;Is there any application note that using two S12ZVM128 for LIN communication?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for reading&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Sep 2017 07:26:29 GMT</pubDate>
    <dc:creator>bjhwang</dc:creator>
    <dc:date>2017-09-18T07:26:29Z</dc:date>
    <item>
      <title>S12ZVM128 EVB LIN communication</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVM128-EVB-LIN-communication/m-p/706020#M14640</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Sir or Madam,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to ask you question about the S12ZVM128 EVB LIN communication.&lt;/P&gt;&lt;P&gt;Currently I have two &lt;SPAN&gt;S12ZVM128 EVB boards and&lt;/SPAN&gt;&amp;nbsp;found two application notes(AN5201, AN5122).&lt;/P&gt;&lt;P&gt;But one is using S12ZVR32EVB for master, a S12ZVM128EVB for slave(AN5201), and the other one uses a S12ZVM EVB as master, S12VR64 EVB as slave(AN5122).&lt;BR /&gt;So I tried to mixed these it up, but it doesn't work.&lt;/P&gt;&lt;P&gt;Is there any application note that using two S12ZVM128 for LIN communication?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for reading&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Sep 2017 07:26:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVM128-EVB-LIN-communication/m-p/706020#M14640</guid>
      <dc:creator>bjhwang</dc:creator>
      <dc:date>2017-09-18T07:26:29Z</dc:date>
    </item>
    <item>
      <title>Re: S12ZVM128 EVB LIN communication</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVM128-EVB-LIN-communication/m-p/706021#M14641</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Please refer to &lt;A href="https://www.nxp.com/downloads/en/device-drivers/FSL_LIN_2.X_STACK.zip"&gt;LIN2.x and SAE J2602 Stack (REV v4.5.9)&lt;/A&gt; which provides examples for both S12ZVML128 master and slave. See the user_guide file in the example folder.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Sep 2017 15:21:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVM128-EVB-LIN-communication/m-p/706021#M14641</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-09-18T15:21:42Z</dc:date>
    </item>
  </channel>
</rss>