<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックCan S12XHZ enter debug mode if it is programmed to boot and operate in special single chip mode with mode switch set to &amp;quot;no&amp;quot; ?</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Can-S12XHZ-enter-debug-mode-if-it-is-programmed-to-boot-and/m-p/696175#M14480</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;An instrument cluster freezes / locks up randomly in a moving vehicle. It got locked up when the truck went over railroad trucks&amp;nbsp;&lt;SPAN style="font-size: 11.0pt;"&gt;or when a trailer was attached via the fifth wheel. It also happened in&amp;nbsp;truck bay with no shock to it.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Could it be that the due to noises in the battery, the S12XHZ enters debug mode and remains stuck at a point until battery is disconnected and connected again ?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 Aug 2017 14:10:32 GMT</pubDate>
    <dc:creator>khusboo</dc:creator>
    <dc:date>2017-08-10T14:10:32Z</dc:date>
    <item>
      <title>Can S12XHZ enter debug mode if it is programmed to boot and operate in special single chip mode with mode switch set to "no" ?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Can-S12XHZ-enter-debug-mode-if-it-is-programmed-to-boot-and/m-p/696175#M14480</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;An instrument cluster freezes / locks up randomly in a moving vehicle. It got locked up when the truck went over railroad trucks&amp;nbsp;&lt;SPAN style="font-size: 11.0pt;"&gt;or when a trailer was attached via the fifth wheel. It also happened in&amp;nbsp;truck bay with no shock to it.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Could it be that the due to noises in the battery, the S12XHZ enters debug mode and remains stuck at a point until battery is disconnected and connected again ?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Aug 2017 14:10:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Can-S12XHZ-enter-debug-mode-if-it-is-programmed-to-boot-and/m-p/696175#M14480</guid>
      <dc:creator>khusboo</dc:creator>
      <dc:date>2017-08-10T14:10:32Z</dc:date>
    </item>
    <item>
      <title>Re: Can S12XHZ enter debug mode if it is programmed to boot and operate in special single chip mode with mode switch set to "no" ?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Can-S12XHZ-enter-debug-mode-if-it-is-programmed-to-boot-and/m-p/696176#M14481</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;It could be anything.&lt;/P&gt;&lt;P&gt;It is possible to flash the MCU with a simple code?&lt;/P&gt;&lt;P&gt;This would tell us this is hardware issue in case the problem remained.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Aug 2017 13:18:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Can-S12XHZ-enter-debug-mode-if-it-is-programmed-to-boot-and/m-p/696176#M14481</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-08-14T13:18:16Z</dc:date>
    </item>
    <item>
      <title>Re: Can S12XHZ enter debug mode if it is programmed to boot and operate in special single chip mode with mode switch set to "no" ?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Can-S12XHZ-enter-debug-mode-if-it-is-programmed-to-boot-and/m-p/696177#M14482</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes it is possible to program the MCU with a simple code. What do you suggest i put in the software and check ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Khusboo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Aug 2017 17:23:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Can-S12XHZ-enter-debug-mode-if-it-is-programmed-to-boot-and/m-p/696177#M14482</guid>
      <dc:creator>khusboo</dc:creator>
      <dc:date>2017-08-14T17:23:26Z</dc:date>
    </item>
    <item>
      <title>Re: Can S12XHZ enter debug mode if it is programmed to boot and operate in special single chip mode with mode switch set to "no" ?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Can-S12XHZ-enter-debug-mode-if-it-is-programmed-to-boot-and/m-p/696178#M14483</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Try to simplify the code, disable a few peripherals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Aug 2017 07:59:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Can-S12XHZ-enter-debug-mode-if-it-is-programmed-to-boot-and/m-p/696178#M14483</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-08-15T07:59:20Z</dc:date>
    </item>
    <item>
      <title>Re: Can S12XHZ enter debug mode if it is programmed to boot and operate in special single chip mode with mode switch set to "no" ?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Can-S12XHZ-enter-debug-mode-if-it-is-programmed-to-boot-and/m-p/696179#M14484</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is a random failure in the trucks and i am unable to reproduce it at my end nor do i&amp;nbsp;have an access to the trucks which is in a far off geographical location.&lt;/P&gt;&lt;P&gt;So, what you suggest, which is a logical step to solving a problem like this one, will not work for me, unfortunately.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Would it be possible for you to provide more information on this special single chip mode. What is there on datasheet is not sufficient.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Aug 2017 18:10:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Can-S12XHZ-enter-debug-mode-if-it-is-programmed-to-boot-and/m-p/696179#M14484</guid>
      <dc:creator>khusboo</dc:creator>
      <dc:date>2017-08-15T18:10:18Z</dc:date>
    </item>
    <item>
      <title>Re: Can S12XHZ enter debug mode if it is programmed to boot and operate in special single chip mode with mode switch set to "no" ?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Can-S12XHZ-enter-debug-mode-if-it-is-programmed-to-boot-and/m-p/696180#M14485</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;In the special single chip mode BDM is enabled and active immediately out of reset. There is a difference in access to several registers. The MCU can enter the mode only out of reset if MODC = 0, MODB = 0, MODC = 0.&lt;/P&gt;&lt;P&gt;I think the MCU goes through reset due to some failure (clock monitor reset, low voltage, cop, illegal address access). And because you have a debugger connected, the MCU enters the special single chip mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Aug 2017 08:32:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Can-S12XHZ-enter-debug-mode-if-it-is-programmed-to-boot-and/m-p/696180#M14485</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-08-16T08:32:57Z</dc:date>
    </item>
  </channel>
</rss>