<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: mc9s12xep100 flash program in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/mc9s12xep100-flash-program/m-p/695213#M14466</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;How do you program the PFlash block?&lt;/P&gt;&lt;P&gt;You cannot execute any flash command from the same PFlash block you want to erase/program. The function should be place in RAM.&lt;/P&gt;&lt;P&gt;Also, check whether the PFlash area is protected or not. In case of a protection violation, FPVIOL flag is set in FSTAT register.&lt;/P&gt;&lt;P&gt;Please see the attached example code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Oct 2017 15:00:54 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2017-10-03T15:00:54Z</dc:date>
    <item>
      <title>mc9s12xep100 flash program</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/mc9s12xep100-flash-program/m-p/695212#M14465</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI, I program rom4000 p-flash is unsuccessful in BDM mode, but I program p-flash block1 is successful. can you give me some technical documents about promgram flash.Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 30 Sep 2017 01:44:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/mc9s12xep100-flash-program/m-p/695212#M14465</guid>
      <dc:creator>chenchenchen</dc:creator>
      <dc:date>2017-09-30T01:44:30Z</dc:date>
    </item>
    <item>
      <title>Re: mc9s12xep100 flash program</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/mc9s12xep100-flash-program/m-p/695213#M14466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;How do you program the PFlash block?&lt;/P&gt;&lt;P&gt;You cannot execute any flash command from the same PFlash block you want to erase/program. The function should be place in RAM.&lt;/P&gt;&lt;P&gt;Also, check whether the PFlash area is protected or not. In case of a protection violation, FPVIOL flag is set in FSTAT register.&lt;/P&gt;&lt;P&gt;Please see the attached example code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Oct 2017 15:00:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/mc9s12xep100-flash-program/m-p/695213#M14466</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-10-03T15:00:54Z</dc:date>
    </item>
  </channel>
</rss>