<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S12ZVC EVALUATION BOARD Schematic question in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVC-EVALUATION-BOARD-Schematic-question/m-p/690924#M14420</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mars,&lt;/P&gt;&lt;P&gt;I cannot see any problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The VDDC is typically used for CAN PHY only.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The VDDX pin behaves as output voltage pin when regulator is configured as internal. When regulator is configured as external, the VDDX pin behaves as input voltage pin.&lt;/P&gt;&lt;P&gt;The VDDX is power supply rail for most of the GPIO pins (port AD is powered from VDDA).&lt;/P&gt;&lt;P&gt;So, the 5V for voltage translator should be connected to the VDDX pin.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Let’s assume that VDDX is configured as internal and MCU consumption itself is 25mA.&lt;/P&gt;&lt;P&gt;The RM specifies that internal regulator may provide up to 70mA (for VSUP&amp;gt;6V, TJ &amp;lt; &lt;SPAN style="font-size: 10.0pt;"&gt;+175&lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;°&lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;C&lt;/SPAN&gt;).&lt;/P&gt;&lt;P&gt;So, there remains up to 45mA for VDDX and pin loads.&lt;/P&gt;&lt;P&gt;Please take these numbers with reserve. The available output current should be evaluated per target application and thermal analysis.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Radek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Jun 2017 09:10:52 GMT</pubDate>
    <dc:creator>RadekS</dc:creator>
    <dc:date>2017-06-20T09:10:52Z</dc:date>
    <item>
      <title>S12ZVC EVALUATION BOARD Schematic question</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVC-EVALUATION-BOARD-Schematic-question/m-p/690921#M14417</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;For S12ZVC evaluation board there are some questions , thank you&lt;BR /&gt;1.VDDA &amp;amp; VDDX &amp;amp; VDDC by external VSUP direct input 12V to internal conversion to 5V?&lt;BR /&gt;2.GPIO &amp;amp; TXD &amp;amp; RXD voltage level is 5V or software can be set to 3.3v? If you need to connect with other ic communication voltage level of 3.3V, how to deal with?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Jun 2017 05:54:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVC-EVALUATION-BOARD-Schematic-question/m-p/690921#M14417</guid>
      <dc:creator>mars_huang</dc:creator>
      <dc:date>2017-06-19T05:54:29Z</dc:date>
    </item>
    <item>
      <title>Re: S12ZVC EVALUATION BOARD Schematic question</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVC-EVALUATION-BOARD-Schematic-question/m-p/690922#M14418</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mars,&lt;/P&gt;&lt;P&gt;The S12ZVC contains VDDX, VDDC regulators. So, we may power MCU directly from 12V.&lt;BR /&gt;The VDDX regulator may be configured as internal (P=(12V-5V)*IDDX must be dissipated by MCU package) or external (P=(12V-5V)*IDDX will be dissipated by external PNP transistor).&lt;BR /&gt;The VDDC regulator does not have the internal option as VDDX (external PNP transistor is needed).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The output voltage from VDDX and VDDC regulators is 5V. &lt;BR /&gt;The selectable output voltage is a feature available only at S12ZVLA128 or S12ZVLA64 MCUs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The optimal solution for 5V / 3V3 interconnection is using voltage translators. For example 74LVC1T45.&lt;BR /&gt;For specific buses might be used dedicated circuits like a PCA9517for I2C bus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I would like to recommend our application note AN2433 5V to 3V Design Considerations&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Ffiles%2Fmicrocontrollers%2Fdoc%2Fapp_note%2FAN2433.pdf" rel="nofollow" target="_blank"&gt;http://www.nxp.com/files/microcontrollers/doc/app_note/AN2433.pdf&lt;/A&gt;&lt;BR /&gt;with general information about this topic. &lt;BR /&gt;Please be aware, that this AN is already 15 years old and the voltage translation portfolio is now much wider.&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nexperia.com%2Fproducts%2Flogic%2Flogic-voltage-translators" rel="nofollow" target="_blank"&gt;https://www.nexperia.com/products/logic/logic-voltage-translators&lt;/A&gt;&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fproducts%2Finterfaces%2Fvoltage-level-translators%3AVOLTAGE-LEVEL-TRANSLATORS" rel="nofollow" target="_blank"&gt;http://www.nxp.com/products/interfaces/voltage-level-translators:VOLTAGE-LEVEL-TRANSLATORS&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Radek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Jun 2017 11:51:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVC-EVALUATION-BOARD-Schematic-question/m-p/690922#M14418</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2017-06-19T11:51:24Z</dc:date>
    </item>
    <item>
      <title>Re: S12ZVC EVALUATION BOARD Schematic question</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVC-EVALUATION-BOARD-Schematic-question/m-p/690923#M14419</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Radek,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; Thank you for your reply, there is a problem, VDDX and VDDC is the internal conversion 5V voltage, then how to provide 5V voltage level to the voltage converter? Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jun 2017 02:55:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVC-EVALUATION-BOARD-Schematic-question/m-p/690923#M14419</guid>
      <dc:creator>mars_huang</dc:creator>
      <dc:date>2017-06-20T02:55:46Z</dc:date>
    </item>
    <item>
      <title>Re: S12ZVC EVALUATION BOARD Schematic question</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVC-EVALUATION-BOARD-Schematic-question/m-p/690924#M14420</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mars,&lt;/P&gt;&lt;P&gt;I cannot see any problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The VDDC is typically used for CAN PHY only.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The VDDX pin behaves as output voltage pin when regulator is configured as internal. When regulator is configured as external, the VDDX pin behaves as input voltage pin.&lt;/P&gt;&lt;P&gt;The VDDX is power supply rail for most of the GPIO pins (port AD is powered from VDDA).&lt;/P&gt;&lt;P&gt;So, the 5V for voltage translator should be connected to the VDDX pin.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Let’s assume that VDDX is configured as internal and MCU consumption itself is 25mA.&lt;/P&gt;&lt;P&gt;The RM specifies that internal regulator may provide up to 70mA (for VSUP&amp;gt;6V, TJ &amp;lt; &lt;SPAN style="font-size: 10.0pt;"&gt;+175&lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;°&lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;C&lt;/SPAN&gt;).&lt;/P&gt;&lt;P&gt;So, there remains up to 45mA for VDDX and pin loads.&lt;/P&gt;&lt;P&gt;Please take these numbers with reserve. The available output current should be evaluated per target application and thermal analysis.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Radek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jun 2017 09:10:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVC-EVALUATION-BOARD-Schematic-question/m-p/690924#M14420</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2017-06-20T09:10:52Z</dc:date>
    </item>
    <item>
      <title>Re: S12ZVC EVALUATION BOARD Schematic question</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVC-EVALUATION-BOARD-Schematic-question/m-p/690925#M14421</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Hi Radek,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I see your reply to other questions (link below) and I always think that the external PNP is the switch, but now it's clear that thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=Https%3A%2F%2Fcommunity.nxp.com%2Fthread%2F437034" rel="nofollow" target="_blank"&gt;Https://community.nxp.com/thread/437034&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jun 2017 10:56:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVC-EVALUATION-BOARD-Schematic-question/m-p/690925#M14421</guid>
      <dc:creator>mars_huang</dc:creator>
      <dc:date>2017-06-20T10:56:36Z</dc:date>
    </item>
    <item>
      <title>Re: S12ZVC EVALUATION BOARD Schematic question</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVC-EVALUATION-BOARD-Schematic-question/m-p/690926#M14422</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Hi Mars,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Thank you for your note. Your previous questions are now clear also for me.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;I am glad that this small misunderstanding was explained.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Best regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Radek&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jun 2017 12:12:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVC-EVALUATION-BOARD-Schematic-question/m-p/690926#M14422</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2017-06-20T12:12:11Z</dc:date>
    </item>
  </channel>
</rss>