<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S12XE &amp; 3.3V supply in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XE-3-3V-supply/m-p/680297#M14248</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;It shouldn’t be a problem. The MCU has Low Voltage Reset (LVR) which forces the device to reset if input voltage is too low, protecting against brown-out condition. LVR assert level is typically 3.02V, deassert at 3.13V (max) see Table A-21.&lt;/P&gt;&lt;P&gt;Evaluation board &lt;A href="http://www.nxp.com/products/automotive-products/microcontrollers-and-processors/16-bit-s12-s12x-mcus/development-board-for-9s12xep100-mcu-evaluation:DEVKIT-S12XE"&gt;DEVKIT-S12XE&lt;/A&gt; uses 3.3V power supply.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Jul 2017 09:11:42 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2017-07-04T09:11:42Z</dc:date>
    <item>
      <title>S12XE &amp; 3.3V supply</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XE-3-3V-supply/m-p/680296#M14247</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a board that uses a S12XE controller and the power supply is 5V.&lt;/P&gt;&lt;P&gt;It has also an atmel flash memory that works at 3.3V&lt;/P&gt;&lt;P&gt;I have to redesign and simplify the board.&lt;/P&gt;&lt;P&gt;Since to board has already power supply of 3.3V, I am thinking of making&amp;nbsp;&lt;SPAN&gt;S12XE controller to work at 3.3V.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The only problem I have is that the specification gives as minimum voltage of VDDR, VDDA 3.13 that is very close to 3.3V (the difference is only 170mV). &lt;/SPAN&gt;&lt;SPAN&gt;For the reset I am going to use&amp;nbsp;LM37XX that keeps uC to reset at the voltage of 3.14V&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I would like to ask if anyone have already used any HCS controller at 3.3V and if he&amp;nbsp;&lt;/SPAN&gt;believe that is save to used power supply so close to minimum voltage.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Jun 2017 13:15:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XE-3-3V-supply/m-p/680296#M14247</guid>
      <dc:creator>Eric_t</dc:creator>
      <dc:date>2017-06-30T13:15:30Z</dc:date>
    </item>
    <item>
      <title>Re: S12XE &amp; 3.3V supply</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XE-3-3V-supply/m-p/680297#M14248</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;It shouldn’t be a problem. The MCU has Low Voltage Reset (LVR) which forces the device to reset if input voltage is too low, protecting against brown-out condition. LVR assert level is typically 3.02V, deassert at 3.13V (max) see Table A-21.&lt;/P&gt;&lt;P&gt;Evaluation board &lt;A href="http://www.nxp.com/products/automotive-products/microcontrollers-and-processors/16-bit-s12-s12x-mcus/development-board-for-9s12xep100-mcu-evaluation:DEVKIT-S12XE"&gt;DEVKIT-S12XE&lt;/A&gt; uses 3.3V power supply.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Jul 2017 09:11:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XE-3-3V-supply/m-p/680297#M14248</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-07-04T09:11:42Z</dc:date>
    </item>
  </channel>
</rss>