<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: mc9s12xep100 MSCAN in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/mc9s12xep100-MSCAN/m-p/676299#M14173</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the issue could be anywhere. Program could be OK (I are absolutely sure there a re no changes) but the system you have put your node into could be different - I do not know, you have not described.&lt;/P&gt;&lt;P&gt;If I were in your shoes I would:&lt;/P&gt;&lt;P&gt;1) check the bus clock and/or oscillator clock to be sure the CAN clock is OK. Also check all the nodes connected to the bus&amp;nbsp; use the same you are connection to&lt;/P&gt;&lt;P&gt;2) test the CAN in the loopback mode to be sure CAN peripheral is OK.&lt;/P&gt;&lt;P&gt;3) test the communication between two CAN nodes at the same MCU without transceiver to be sure the communication is OK. The circuit can be found &lt;A class="link-titled" href="https://www.mikrocontroller.net/attachment/28831/siemens_AP2921.pdf" title="https://www.mikrocontroller.net/attachment/28831/siemens_AP2921.pdf"&gt;https://www.mikrocontroller.net/attachment/28831/siemens_AP2921.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In this case I would also measure the CAN signal by the scope whether the communication speed is OK.&lt;/P&gt;&lt;P&gt;4) If the everything above is OK then the issue is on the transceiver side and/or BUS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know, it is easy to write it but difficult to test. However, it is necessary to go step by step to exclude possible sources of issues.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ladislav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Jul 2017 09:10:20 GMT</pubDate>
    <dc:creator>lama</dc:creator>
    <dc:date>2017-07-20T09:10:20Z</dc:date>
    <item>
      <title>mc9s12xep100 MSCAN</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/mc9s12xep100-MSCAN/m-p/676298#M14172</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi，I have some problem with MSCAN. I run a program to test MSCAN,but the&amp;nbsp;CAN0CTL0_SYNCH bit is always is 0, so MSCAN can not transmit anything. And I am sure that the program is right,beause run this program sucessfully in other board. So, I want to know what about reasons cause this. &amp;nbsp;Is hardware cuased this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jul 2017 07:25:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/mc9s12xep100-MSCAN/m-p/676298#M14172</guid>
      <dc:creator>chenchenchen</dc:creator>
      <dc:date>2017-07-20T07:25:04Z</dc:date>
    </item>
    <item>
      <title>Re: mc9s12xep100 MSCAN</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/mc9s12xep100-MSCAN/m-p/676299#M14173</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the issue could be anywhere. Program could be OK (I are absolutely sure there a re no changes) but the system you have put your node into could be different - I do not know, you have not described.&lt;/P&gt;&lt;P&gt;If I were in your shoes I would:&lt;/P&gt;&lt;P&gt;1) check the bus clock and/or oscillator clock to be sure the CAN clock is OK. Also check all the nodes connected to the bus&amp;nbsp; use the same you are connection to&lt;/P&gt;&lt;P&gt;2) test the CAN in the loopback mode to be sure CAN peripheral is OK.&lt;/P&gt;&lt;P&gt;3) test the communication between two CAN nodes at the same MCU without transceiver to be sure the communication is OK. The circuit can be found &lt;A class="link-titled" href="https://www.mikrocontroller.net/attachment/28831/siemens_AP2921.pdf" title="https://www.mikrocontroller.net/attachment/28831/siemens_AP2921.pdf"&gt;https://www.mikrocontroller.net/attachment/28831/siemens_AP2921.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In this case I would also measure the CAN signal by the scope whether the communication speed is OK.&lt;/P&gt;&lt;P&gt;4) If the everything above is OK then the issue is on the transceiver side and/or BUS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know, it is easy to write it but difficult to test. However, it is necessary to go step by step to exclude possible sources of issues.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ladislav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jul 2017 09:10:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/mc9s12xep100-MSCAN/m-p/676299#M14173</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2017-07-20T09:10:20Z</dc:date>
    </item>
  </channel>
</rss>