<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 S12ZVM PMF internal signal</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVM-PMF-internal-signal/m-p/673593#M14138</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a question about S12ZVM PMF internal signal.&lt;/P&gt;&lt;P&gt;I refer S12ZVM RM rev2.11.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is the description on Chapter15(PMF) that&lt;/P&gt;&lt;P&gt;"pmf_reload_is_async" serves as a qualifier to the PMF reload event signal "pmf_reloada".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the other hand, there is another description on Chapter1 Figure 1-9. Internal Control Loop Configuration&lt;/P&gt;&lt;P&gt;that "reload"&amp;nbsp;and "async_reload" signals outputs from PMF modules.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can understand two patterns as follows.&lt;/P&gt;&lt;P&gt;1) "reload" = "pmf_reloada"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; "async_reload" = "pmf_reload_is_async"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) "reload" = "pmf_reloada"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; "async_reload" = "pmf_reloada" ^ "pmf_reload_is_async" (&lt;SPAN lang="en"&gt;logical conjunction)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which is correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Ikki&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 May 2017 13:29:55 GMT</pubDate>
    <dc:creator>ikkishingu</dc:creator>
    <dc:date>2017-05-09T13:29:55Z</dc:date>
    <item>
      <title>S12ZVM PMF internal signal</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVM-PMF-internal-signal/m-p/673593#M14138</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a question about S12ZVM PMF internal signal.&lt;/P&gt;&lt;P&gt;I refer S12ZVM RM rev2.11.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is the description on Chapter15(PMF) that&lt;/P&gt;&lt;P&gt;"pmf_reload_is_async" serves as a qualifier to the PMF reload event signal "pmf_reloada".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the other hand, there is another description on Chapter1 Figure 1-9. Internal Control Loop Configuration&lt;/P&gt;&lt;P&gt;that "reload"&amp;nbsp;and "async_reload" signals outputs from PMF modules.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can understand two patterns as follows.&lt;/P&gt;&lt;P&gt;1) "reload" = "pmf_reloada"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; "async_reload" = "pmf_reload_is_async"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) "reload" = "pmf_reloada"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; "async_reload" = "pmf_reloada" ^ "pmf_reload_is_async" (&lt;SPAN lang="en"&gt;logical conjunction)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which is correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Ikki&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 May 2017 13:29:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVM-PMF-internal-signal/m-p/673593#M14138</guid>
      <dc:creator>ikkishingu</dc:creator>
      <dc:date>2017-05-09T13:29:55Z</dc:date>
    </item>
    <item>
      <title>Re: S12ZVM PMF internal signal</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVM-PMF-internal-signal/m-p/673594#M14139</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ikki,&lt;/P&gt;&lt;P&gt;I agree, that these internal signals descriptions in RM are quite confusing. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The pmf_reloada signal is routed into PTU module. Therefore:&lt;/P&gt;&lt;P&gt;"reload" signal = "pmf_reloada" signal&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The "pmf_reload_is_async" signal is also routed into PTU module. Therefore:&lt;/P&gt;&lt;P&gt;"async_reload" signal = "pmf_reload_is_async" signal&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The pmf_reloada signal is generated at specified PWM opportunity (see chapter 15.4.12.3 Load Frequency) = at a start of control loop cycle.&lt;/P&gt;&lt;P&gt;The pmf_reload_is_async signal is generated when async_event (named also “commutation_event”, generated by TIM0_OC0) is detected.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the PTU is enabled the reload and async_reload events are immediately passed through to the ADC and GDU modules.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the restart is enabled (RSTRTx=1), the commutation event generates both “PWM reload event” and “PWM reload-is-asynchronous event” simultaneously except the case when the asynchronous event and generated PWM reload event occur in the same cycle (only “PWM reload event” is generated).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The PWM restart at commutation event is used for BLDC Six-Step Commutation driving (for both Hall/sensorless).&lt;/P&gt;&lt;P&gt;For example:&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&amp;nbsp; PMFENCA_RSTRTA &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// 1 = PWM restart at commutation event‍‍&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Radek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 May 2017 13:19:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVM-PMF-internal-signal/m-p/673594#M14139</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2017-05-11T13:19:17Z</dc:date>
    </item>
    <item>
      <title>Re: S12ZVM PMF internal signal</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVM-PMF-internal-signal/m-p/673595#M14140</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Radek,&lt;/P&gt;&lt;P&gt;Thank you for your reply and I am sorry for the delay in my response.&lt;/P&gt;&lt;P&gt;From your comment, I&amp;nbsp;understand 1) is correct as proper understanding.&lt;/P&gt;&lt;P&gt;Best Regards.&lt;/P&gt;&lt;P&gt;Ikki&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 May 2017 08:43:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12ZVM-PMF-internal-signal/m-p/673595#M14140</guid>
      <dc:creator>ikkishingu</dc:creator>
      <dc:date>2017-05-30T08:43:51Z</dc:date>
    </item>
  </channel>
</rss>