<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: can i use execute function code in ram ? in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/can-i-use-execute-function-code-in-ram/m-p/673211#M14137</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Byeongjin,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When you will define some function directly on RAM like your original proposal, the function will be compiled for work in RAM and automatically copy from Flash to the RAM during Startup() – like variable initialization. For example:&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="property macro token"&gt;#pragma CODE_SEG DEFAULT_RAM&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;MY_Function&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp; &lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#pragma CODE_SEG DEFAULT‍‍‍‍‍‍&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please be aware that the same #pragmas must be used also for function prototype.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The next option is compiling code for run in RAM and copy it there manually – as it is used in your next post (using RELOCATE_TO qualifier in prm linker file).&lt;/P&gt;&lt;P&gt;In that case, you should create a function which will copy ToCopyToRam section to the RAM (starting from 0x2000).&lt;/P&gt;&lt;P&gt;For example:&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="keyword token"&gt;static&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;CopyCodeToRAM&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt; 
&amp;nbsp; UINT8 &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;Src&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp; UINT8 &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;Dst&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp; UINT16&amp;nbsp; SegSize&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp; UINT16&amp;nbsp; x&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 
&amp;nbsp; &lt;SPAN class="comment token"&gt;//RAM code resides in Flash from 0xFFEE00 to 0xFFFDFF&lt;/SPAN&gt;
&amp;nbsp; Src &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;UINT8 &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="token function"&gt;__SEG_START_REF&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;ToCopyToRam&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp; Dst &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;UINT8 &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x2000&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;//copied to RAM at 0x2000&lt;/SPAN&gt;
&amp;nbsp; SegSize &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;UINT16&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="token function"&gt;__SEG_SIZE_REF&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;ToCopyToRam&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 
&amp;nbsp; &lt;SPAN class="keyword token"&gt;for&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;x &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; x &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt; SegSize&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; x&lt;SPAN class="operator token"&gt;++&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;//just copy a byte at a time&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;Dst&lt;SPAN class="operator token"&gt;++&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;Src&lt;SPAN class="operator token"&gt;++&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Radek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Jul 2017 11:13:00 GMT</pubDate>
    <dc:creator>RadekS</dc:creator>
    <dc:date>2017-07-21T11:13:00Z</dc:date>
    <item>
      <title>can i use execute function code in ram ?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/can-i-use-execute-function-code-in-ram/m-p/673208#M14134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I develop motor control software.&amp;nbsp;&lt;/P&gt;&lt;P&gt;i use&amp;nbsp;PTU interrupt. (ADC end interrupt)&lt;/P&gt;&lt;P&gt;The code size becomes large, and it takes a long time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can this processor be copied to RAM and run?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The motor controller code has already been developed on the TI MCU (C28xx). (Verified code)&lt;/P&gt;&lt;P&gt;Changing MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;--------------------------&lt;/P&gt;&lt;P&gt;example)&lt;/P&gt;&lt;P&gt;#pragma CODE_SEG DEFAULT_RAM&lt;/P&gt;&lt;P&gt;void MY_Function(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; .....&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;#pragma CODE_SEG DEFAULT&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"Events.c"&lt;/P&gt;&lt;P&gt;void AD2_OnEnd(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;SPAN&gt;MY_Function();&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;--------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is it right? but compile error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- CodeWarrior 10.7 (using PE)&lt;/P&gt;&lt;P&gt;- S12ZVMC128&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Jul 2017 11:17:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/can-i-use-execute-function-code-in-ram/m-p/673208#M14134</guid>
      <dc:creator>byeongjinkim</dc:creator>
      <dc:date>2017-07-18T11:17:57Z</dc:date>
    </item>
    <item>
      <title>Re: can i use execute function code in ram ?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/can-i-use-execute-function-code-in-ram/m-p/673209#M14135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Byeongjin,&lt;/P&gt;&lt;P&gt;Yes, you can use such construction. That is simplest method.&lt;/P&gt;&lt;P&gt;It works correctly on my side. I created new PE project with ADC and I placed MY_Function() code at start of Events.c file.&lt;/P&gt;&lt;P&gt;Could you please let mi know which compiler error you got?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note: If this should be time critical task, there are two unwanted function calls (The AD1_Interrupt calls AD1_OnEnd() which calls MY_Function()) which will degrade execution time by stacking/unstacking.&lt;/P&gt;&lt;P&gt;I would like to recommend taking PE code just like inspiration and wrote ADC interrupt routine manually.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You may also inspire at our NXP official example codes:&lt;/P&gt;&lt;P&gt;3-Phase Hall Sensor BLDC S12ZVM Application – six step driving&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/docs/en/user-guide/MTRCKTSBNZVMHQSG.pdf"&gt;http://www.nxp.com/docs/en/user-guide/MTRCKTSBNZVMHQSG.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/docs/en/application-note/AN4718.pdf"&gt;http://www.nxp.com/docs/en/application-note/AN4718.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/docs/en/application-note-software/AN4718SW.zip"&gt;http://www.nxp.com/docs/en/application-note-software/AN4718SW.zip&lt;/A&gt;&lt;/P&gt;&lt;P&gt;3-Phase Sensorless BLDC S12ZVM Application – six step driving&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/docs/en/user-guide/MTRCKTSBNZVM128QSG.pdf"&gt;http://www.nxp.com/docs/en/user-guide/MTRCKTSBNZVM128QSG.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/docs/en/application-note/AN4704.pdf"&gt;http://www.nxp.com/docs/en/application-note/AN4704.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/downloads/en/board-support-packages/MTRCKTSBNZVM128_SW.exe"&gt;http://www.nxp.com/downloads/en/board-support-packages/MTRCKTSBNZVM128_SW.exe&lt;/A&gt;&lt;/P&gt;&lt;P&gt;3-phase Sensorless Dual-Shunt PMSM S12ZVM Application – FOC driving&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/docs/en/user-guide/MTRCKTSPNZVM128QSG.pdf"&gt;http://www.nxp.com/docs/en/user-guide/MTRCKTSPNZVM128QSG.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/docs/en/application-note/AN5135.pdf"&gt;http://www.nxp.com/docs/en/application-note/AN5135.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/downloads/en/evaluation-development-boards-systems/MTRCKTSPNZVM128_SW.exe"&gt;http://www.nxp.com/downloads/en/evaluation-development-boards-systems/MTRCKTSPNZVM128_SW.exe&lt;/A&gt;&lt;/P&gt;&lt;P&gt;3-phase Sensorless Single-Shunt PMSM S12ZVM Application – FOC driving&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/docs/en/application-note/AN5327.pdf"&gt;http://www.nxp.com/docs/en/application-note/AN5327.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/assets/documents/data/en/user-guides/AN5327-QSG.pdf"&gt;http://www.nxp.com/assets/documents/data/en/user-guides/AN5327-QSG.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Note: please be aware that there is still typo error in this document (already reported) – the jumpers J57 and J60 should be in position 2-3.&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/docs/en/application-note-software/AN5327SW.zip"&gt;http://www.nxp.com/docs/en/application-note-software/AN5327SW.zip&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note: We should avoid using float type since MCU do not have hardware support for that. The software emulation takes too long.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note: The computation window may be extended by PMFFQCA_LDFQA[3:0] bit configuration. This field selects the PWM load frequency – Every 1..16 PWM opportunities.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Radek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jul 2017 11:09:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/can-i-use-execute-function-code-in-ram/m-p/673209#M14135</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2017-07-20T11:09:52Z</dc:date>
    </item>
    <item>
      <title>Re: can i use execute function code in ram ?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/can-i-use-execute-function-code-in-ram/m-p/673210#M14136</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;change to PWM reload interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/26884i7A477E3344ED8B8E/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;how to executing in ram? Do I need to copy all the memory?&lt;/P&gt;&lt;P&gt;&amp;nbsp;ToCopyToRam(0xFFEE00 ~ 0xFFFDFF) ㅡ&amp;gt; (0x002000 ~ 0x002FFF)&lt;/P&gt;&lt;P&gt;all copy?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jul 2017 05:22:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/can-i-use-execute-function-code-in-ram/m-p/673210#M14136</guid>
      <dc:creator>byeongjinkim</dc:creator>
      <dc:date>2017-07-21T05:22:42Z</dc:date>
    </item>
    <item>
      <title>Re: can i use execute function code in ram ?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/can-i-use-execute-function-code-in-ram/m-p/673211#M14137</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Byeongjin,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When you will define some function directly on RAM like your original proposal, the function will be compiled for work in RAM and automatically copy from Flash to the RAM during Startup() – like variable initialization. For example:&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="property macro token"&gt;#pragma CODE_SEG DEFAULT_RAM&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;MY_Function&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp; &lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#pragma CODE_SEG DEFAULT‍‍‍‍‍‍&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please be aware that the same #pragmas must be used also for function prototype.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The next option is compiling code for run in RAM and copy it there manually – as it is used in your next post (using RELOCATE_TO qualifier in prm linker file).&lt;/P&gt;&lt;P&gt;In that case, you should create a function which will copy ToCopyToRam section to the RAM (starting from 0x2000).&lt;/P&gt;&lt;P&gt;For example:&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="keyword token"&gt;static&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;CopyCodeToRAM&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt; 
&amp;nbsp; UINT8 &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;Src&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp; UINT8 &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;Dst&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp; UINT16&amp;nbsp; SegSize&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp; UINT16&amp;nbsp; x&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 
&amp;nbsp; &lt;SPAN class="comment token"&gt;//RAM code resides in Flash from 0xFFEE00 to 0xFFFDFF&lt;/SPAN&gt;
&amp;nbsp; Src &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;UINT8 &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="token function"&gt;__SEG_START_REF&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;ToCopyToRam&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp; Dst &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;UINT8 &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x2000&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;//copied to RAM at 0x2000&lt;/SPAN&gt;
&amp;nbsp; SegSize &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;UINT16&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="token function"&gt;__SEG_SIZE_REF&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;ToCopyToRam&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 
&amp;nbsp; &lt;SPAN class="keyword token"&gt;for&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;x &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; x &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt; SegSize&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; x&lt;SPAN class="operator token"&gt;++&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;//just copy a byte at a time&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;Dst&lt;SPAN class="operator token"&gt;++&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;Src&lt;SPAN class="operator token"&gt;++&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Radek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jul 2017 11:13:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/can-i-use-execute-function-code-in-ram/m-p/673211#M14137</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2017-07-21T11:13:00Z</dc:date>
    </item>
  </channel>
</rss>